STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unexpected readings (2X or 0.5X) using ADC on STM32F0

Posted on November 10, 2014 at 20:07 I'm using the ADC on a STM32F072RBT6 to read a constant voltage that is derived from my supply voltage. Sometimes, I get a reading that is twice the expected value, and sometimes I get a reading that is half ...

Stm32f407 PPI communication with BLACK fin

Posted on November 10, 2014 at 13:16I want to write a code for PPI communication between stm32f407 and Blackfin .The code for blackfin I have got from open source...But I dont know how to write the same for stm32f407.Anybody have experience in doing...

sanjib by Associate III
  • 755 Views
  • 0 replies
  • 0 kudos

STORAGE_IsReady_HS() function contains garbage

Posted on September 23, 2014 at 01:55Hi AllCube 4.3.1/Keil/F4:When generating a cube project that includes a USB(HS) mass storage driver, if the file ''USBD_Storage_if.c'' already exists in your project AND has been modified within *USER CODE BEGIN*...

Using Internal Reference for ADC measurements

Posted on November 09, 2014 at 20:07Hi,I would like to use the internal reference (1,2 v) for ADC measurements on a STM32L151CC MCU ( 48 pin ). Is it possible? Thanks for your help.BR Per #internal-reference-adc

per23 by Associate
  • 890 Views
  • 1 replies
  • 0 kudos

GPIO_ToggleBits(GPIOD,GPIO_Pin_9);

Posted on November 09, 2014 at 12:46Dear All,I am using CMSIS '' STM32F0-Discovery_FW_V1.0.0 '' library files for STM32F0 MCU programming which does not support GPIO_ToggleBits(GPIOD,GPIO_Pin_9); instructionI already checked the ''gpio'' file which ...

pic_micro by Associate II
  • 1584 Views
  • 2 replies
  • 0 kudos

How Disable global interrupt with ARM 32F0

Posted on November 02, 2014 at 08:15Dear AllFollowing syntax does nit disable the global interruptPlease advice  uint32_t PriMask = 0x01; //void __enable_irq (void);//Global Interrupt enable (using the instruction CPSIE i) void __set_PRIMASK (uint32...

pic_micro by Associate II
  • 3993 Views
  • 10 replies
  • 0 kudos

Apparent bug in CubeMX clock generation

Posted on November 08, 2014 at 01:47 I seem to have found a bug in the clock configuration of the CubeMX software (Version 4.4.0, the latest as far as I can tell). On an STM32F407, I am setting the SYSCLK to use the PLL with the PLL source being...

mjones by Associate
  • 2529 Views
  • 2 replies
  • 0 kudos