2014-04-08 2:36 AM
I wrote this program, but after I uploaded and connect RS232 to my notebook, Putty didn't show anything, what the problem?
The source code is down blow:
 #include ''stm32f4xx.h'' // Device header
#include <stdio.h>
#include ''misc.h''
#include ''stm32f4xx_usart.h'' // Keil::Device:StdPeriph Drivers:USART
void
STM_EVAL_COMInit(USART_InitTypeDef* USART_InitStruct)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable GPIO clock */
//RCC_AHB1PeriphClockCmd(UART4_TX_PIN | UART4_RX_PIN, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); 
//clock a PORTC
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE); 
//clock alla UART4!
/* Connect PXx to USARTx_Tx*/
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6);
/* Connect PXx to USARTx_Rx*/
GPIO_PinAFConfig( GPIOC, GPIO_PinSource7, GPIO_AF_USART6);
/* Configure USART Tx as alternate function */
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Configure USART Rx as alternate function */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* USART configuration */
USART_Init(USART6, USART_InitStruct);
/* Enable USART */
USART_Cmd(USART6, ENABLE);
}
int
main(
void
){
USART_InitTypeDef Usart6;
Usart6.USART_BaudRate = 38400;
Usart6.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
Usart6.USART_Mode = USART_Mode_Tx;
Usart6.USART_Parity = USART_Parity_No;
Usart6.USART_StopBits = USART_StopBits_1;
Usart6.USART_WordLength = USART_WordLength_8b;
STM_EVAL_COMInit(&Usart6);
USART_ClearFlag(USART6, USART_FLAG_TC);
USART_ClearITPendingBit(USART6,USART_IT_TXE); 
while
(1){
USART_ClearITPendingBit(USART6,USART_IT_TXE); 
USART_SendData(USART6, (uint16_t)
''Testing...\n''
);
while
(USART_GetFlagStatus(USART6, USART_FLAG_TXE) == RESET);
USART_ClearFlag(USART6, USART_FLAG_TC);
}
return
0;
}2014-04-08 2:40 AM
When I see my debug screen, the Data Register is always empty. I don't know this is problem or not.
2014-04-08 4:55 AM
USART_SendData() does not send strings.
int main(void){
USART_InitTypeDef Usart6;
Usart6.USART_BaudRate = 38400;
Usart6.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
Usart6.USART_Mode = USART_Mode_Tx;
Usart6.USART_Parity = USART_Parity_No;
Usart6.USART_StopBits = USART_StopBits_1;
Usart6.USART_WordLength = USART_WordLength_8b;
STM_EVAL_COMInit(&Usart6);
while(1){
while(USART_GetFlagStatus(USART6, USART_FLAG_TXE) == RESET);
USART_SendData(USART6, 0x54);
}
return 0;
}2014-04-08 5:33 AM
// STM32 USART6 ECHO (Tx PC.6, Rx PC.7) STM32F4DIS-BB - sourcer32@gmail.com
#include ''stm32f4xx.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART6 clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6, ENABLE);
/* GPIOC clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; // PC.6 USART6_TX, PC.7 USART6_RX
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_USART6);
}
/**************************************************************************************/
void USART6_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 38400 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 38400;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART6, &USART_InitStructure);
USART_Cmd(USART6, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART6_Configuration();
while(1) // Don't want to exit
{
uint16_t Data;
while(USART_GetFlagStatus(USART6, USART_FLAG_RXNE) == RESET); // Wait for Char
Data = USART_ReceiveData(USART6); // Collect Char
while(USART_GetFlagStatus(USART6, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART6, Data); // Echo Char
}
}
/**************************************************************************/
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d
'', file, line) */
while (1)
{}
}
#endif
/**************************************************************************/2014-04-08 4:46 PM
Thank you very much for your help!
But how can I send a string? I saw somebody use printf(), is that right?2014-04-08 5:29 PM
But how can I send a string? I saw somebody use printf(), is that right?
One character at a time.void USART_putchar(char ch)
{
while(USART_GetFlagStatus(USART6, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART6, ch);
}
void USART_puts(char *s)
{
while(*s)
USART_putchar(*s++);
}2014-04-09 12:11 AM
Thank you for your help. But I still can't see any result on my Putty. I think it because my USB to RS232 line is not comptiable with this board. I use a line with Prolific chip. Will this effect the result?
2014-04-09 1:15 AM
But I still can't see any result on my Putty. I think it because my USB to RS232 line is not comptiable with this board. I use a line with Prolific chip. Will this effect the result?
Usually not. The driver chip/vendor matters only to the PC side, which needs a matching driver (Prolific USB drivers caused bluescreens on a Win7 machine I tried recently). Have you set proper baudrates, including matching startbit, stopbit, parity and handshake settings on both sides ? Have you attached a scope, to check the actual communication ?
2014-04-09 2:55 AM
I will check it out! Thank you!
2014-04-09 7:37 AM
Use a scope and confirm the bit timing.
Directly to the Prolific chip should be fine, used them myself, be careful using the term ''RS232'' as it implies voltage/signalling levels which are not compatible with the STM32. Finally watch where your source code is pulled from, the STM32F4-DISCO uses an 8 MHz external clock, the definition of HSE_VALUE in the project, and the PLL settings in system_stm32f4xx.c need to be coherent with this. The EVAL series boards use 25 MHz crystals, and a lot of the firmware library code assumes this.