STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f4Cube integration with Ride 7?

Posted on June 07, 2014 at 13:18I use the Ride 7 IDE, and have just updated it so I can migrate from STM32f1 to STM32f4 - but cannot find how to integrate Cube into the IDE.  It is supposed to be compatible but I can find no installation instruction...

mike2399 by Associate II
  • 5079 Views
  • 11 replies
  • 0 kudos

Why STM32CUBE!

Posted on November 25, 2014 at 09:01Why doesnt STM32CUBE have any usb sample codes for stm32f4-discovery? Discovery has a usb port on. Everybody know that Virtual Com USB is very slow even 8bit Microchips have Bulk Usb code support about 1024kb/s

mrjaner by Associate II
  • 2845 Views
  • 6 replies
  • 0 kudos

Does the STM32F429 work with Discover-MO DM-STF4BB?

Posted on November 24, 2014 at 22:37I'm new around here and still not sure where all of the information I seek can be found. Any help is most appreciated!That would be (AFAIK) MBMB1075 B-01 and DM-STF4BB if those are more meaningful designations.I h...

hbarta2 by Associate III
  • 2056 Views
  • 5 replies
  • 0 kudos

USB isr breaks interrupt vector in STM32L1

Posted on November 24, 2014 at 14:45Hi everyone, I'm using the STM32L151C6 I have a program, running well, debugging with the ST-Link on IAR. My problem is that as soon as I branch the USB_LP_IRQHandler IRQ to an existing function ( USB_Istr() ) in ...

Kuikui by Associate III
  • 867 Views
  • 1 replies
  • 0 kudos

STM32F4 - read timer value

Posted on November 24, 2014 at 17:27 Hi, I have this timer void InitializeTimer(void) { TIM_TimeBaseInitTypeDef timerInitStructure; NVIC_InitTypeDef NVIC_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); timerInitS...

pano by Associate II
  • 1631 Views
  • 3 replies
  • 0 kudos

Multiple ADC's on STM32F0

Posted on March 30, 2014 at 19:25Hello, I have been having some trouble initializing multiple ADC on my STM32F0 discovery board. I need to sample 4 ADC at a time (or at least one after the other). Does anyone have some example code for initializing ...

shrum by Associate
  • 1402 Views
  • 3 replies
  • 0 kudos

STM32F0 EXTI not triggering

Posted on November 24, 2014 at 21:35Code is very simple. I have checked it again and again but cannot get the interrupt to trigger. The interrupt does trigger if I use the software interrupt command. Anybody see the bug? I am outputting a 150Hz 3.3V...

STM32F4 Discovery CAN pin config

Posted on December 04, 2012 at 18:48Dear all,I am looking forward solution of my problem. I have successfully configured CAN driver in loopback mode, but when I want to connect to physical layer (MCP2551 I/C), there is no output on pins.#define CANx...

mrazek by Associate II
  • 3308 Views
  • 6 replies
  • 0 kudos