STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDADC2 synchronization with SDADC1

Posted on November 26, 2014 at 10:43I have seen a lost of discussions about synchronized sampling of ADCs. But I haven't seen a single example for synchronized sampling of SDADCs anywhere. I am using stm32f373 MCU where I want to sample SDADC1 and S...

rizwin by Associate II
  • 1242 Views
  • 2 replies
  • 0 kudos

ARM32F Unaligned Data Support

Posted on November 25, 2014 at 18:55Dear All,As we can see in the attached picture the ARM support Unaligned and Aligned data supportPlease advice what mechanism is using by arm to identify two or three or four operand at single memory address 

0690X00000602vdQAA.jpg
pic_micro by Associate II
  • 2879 Views
  • 9 replies
  • 0 kudos

IAR : 32 bits SP is not 64 bits DP !

Posted on November 26, 2014 at 14:27Reading http://www.iar.com/Global/Resources/Developers_Toolbox/C_Cplusplus_Programming/Improve_performance_of_digital_signal_processing_with_IAR_Embedded_Workbench_for_ARM.pdfpage 3 :arm_sqrt_f32 : 52 cyclessqrt :...

tarzan2 by Senior
  • 1622 Views
  • 3 replies
  • 0 kudos

Exclamation mark breakpoint

Posted on November 26, 2014 at 18:20 Hi! Keil  MDK Lite V5.12 I cannot tell why the debugger cannot breakpoint certain rows. Like a CAN_Transmit function. Not only will put an exclamation mark, it will jump over it completely. This function is that ...

zamolan by Associate II
  • 1641 Views
  • 1 replies
  • 0 kudos

CHINA made stm32 quality

Posted on November 25, 2014 at 09:09I get some stm32f103cbt6 or similar parts from china that prices are very low compared to digikey prices(ST price is 2.4$ @10000), but china price is about 2$, what is the reason? Is china made stm32 reliable and ...

STM32F4 Disc - delay fuction

Posted on November 26, 2014 at 14:37 Hi, a delay fuction like delay(1000000) how long is? 1000000 what is it? us? ms? thanks

pano by Associate II
  • 1189 Views
  • 1 replies
  • 0 kudos

STM32 Reciprocal Counter

Posted on June 24, 2014 at 09:04I'm trying to make reciprocal counter on STM32F4-Discovery. Concept: 0. Input signal connected to TIM1_Ch1 (PA8) and TIM4_ETR (PE0); 1. TIM1 is clocked from HSE 168MHz,               configured to start from external ...

STM32F4 extending the heap to seperate RAM regions

Posted on November 25, 2014 at 15:39Hello everyone,we got a project where we need literally any space available for dynamic heap allocation.So we now switched from a F2 to a F4 setup, because it has more RAM. We are using the STM32F427 at the moment...