STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L0 GPIOA_MODER A4 default value

Posted on January 06, 2015 at 11:20Hello, the STM32L0 series sets nearly all GPIO to analog mode as default. This does make sense opposed to the ''default to input'' on other family that may result in high current draw with floating inputs. Only Por...

SPI input value being interpreted incorrectly

Posted on January 04, 2015 at 04:11My project involves using a STM32L152 part as a SPI master that receives data from a slave (digital accelerometer). When I look at the SPI signals through a scope, I notice that the incoming SPI data is being inter...

bnp979 by Associate III
  • 4709 Views
  • 5 replies
  • 0 kudos

STM32F4 Discovery and gnu

Posted on January 05, 2015 at 14:21I have a new STM32f4 Discovery board and would like to be able to build, burn, debug programs in Ubuntu linux version 14.04. I basically followed these directions: http://www.wolinlabs.com/blog/linux.stm32.discover...

bobslf by Associate
  • 1356 Views
  • 1 replies
  • 0 kudos

configure LSE for RTC on a STM32F4DISCOVERY board.

Posted on January 01, 2015 at 09:39Hello, hapy 2015 to all. I try to use an external LSE for RTC a STM32F4DISCOVERY . I follow indication of clive1 on this post: https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder...

stm32f4 by Associate II
  • 2394 Views
  • 4 replies
  • 0 kudos

STM32F103C8T6 run after core reset only

Posted on January 04, 2015 at 17:09hi, STM32F103C8T6 Minimum Board after system reset NRST or power reset not run(blink LED). After core reset in ST-Link utility window MCU runs to next hardware button reset. Can any help me please #reset-stm32

HardFault_Handler debugging

Posted on January 04, 2015 at 09:22Dear friends.My platform is STM32F429Discovery.I encountered whit Hard Fault error. I used the code of Joseph Yiu to track the place where error occurs. It is in the portasm_cm4.s (FreeRTOS). ldr r0, [r1]r1=0x03FF...

baev_al by Associate III
  • 979 Views
  • 1 replies
  • 0 kudos

Program always jump to/boot from 0x20000000?

Posted on January 03, 2015 at 13:50Hello all, I just began working on an old project which had some problems that had not been solved, of which I did manage to pinpoint (in relative terms) the source. Developing platform: Keil uv4 Chip:             ...

DAC Internal Reference Settling Time

Posted on January 04, 2015 at 13:09We are building a digital LED buck converter with slope compensation as described AN4885 High brightness LED dimming using the STM32F334 Discovery kit.The discovery kit application uses the DAC to generate a 250 kH...

DAC as internal reference only

Posted on December 28, 2014 at 22:41Does anyone know if it's possible to enable the DAC without having it drive the corresponding output pin (PA4 on STM32F301 in my case)? I want to use it as a reference for the internal comparator, but unfortunatel...

bainorama by Associate II
  • 1001 Views
  • 1 replies
  • 0 kudos