cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 4.2.0 Known Issues

joe
Associate III
Posted on June 11, 2014 at 12:56

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
jeucojeuco
Associate II
Posted on June 12, 2014 at 08:33

This bug isn't only for software STM32CubeMX 4.2.0 but for library STM32Cube F4 v1.1.0

HAL_xxx_CLEAR_IT( ) macro is incorrect

TIMER, ADC, I2C, SPI, TIM, UART, USART, WWDG

=====

https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Java%2fSTM32F4xx%20HAL_TIM_IRQHandler%20misses%20interrupts%20on%20nearly%20overlapping%20TIM%20interrupts&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E...

shippo
Associate II
Posted on June 14, 2014 at 19:41

I found another bug:

When configuring SPI (at least SPI3, I didn't test the others) the generated code fails because hspi3.Init.CRCPolynomial is not set, which leads to a failed assertion in HAL_SPI_Init.

edit:

Also, when MCO2 is configured with PLLI2SCLK as source, no code for the PLLI2S configuration is created, if no I2S instance is configured.
whg03
Associate II
Posted on June 17, 2014 at 18:03

Initialization of ADC1 for SRM32F401RE fails because multimode.DMAAccessMode is not set in in main.c function MX_ADC1_Init().

This causes assert_param() to fail in HAL_ADCEx_MultiModeConfigChannel().