STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM324x9I-Eval : Trace Configuration

Posted on February 23, 2015 at 23:53Hello everyone,I juste received an ulinkpro so I can use the ETM feature later on in my development.  Right now, I am trying to simply display a variable in the logic analyzer but I get no synchronization.  I read...

keaven by Associate II
  • 1270 Views
  • 3 replies
  • 0 kudos

external sdram connection to stm32f429ii

Posted on December 05, 2014 at 19:19Hi,i'd like to connect an external sdram to stm32f429ii controller. There is a question, is it necessary to use dqm pins?  i want to use MT48LC4M32B2 sdram.

Quadrature Encoder STM32 Z Capture

Posted on February 23, 2015 at 15:03 Hello,I'd like to use an quadrature encoder connected to my STM32F4 Discovery Board.I have connected the A and B outputs to PC6 and PC7. CH1 and CH2 of TIM8.It works pretty good, the timer counts.Now I'd like to...

arapp1990 by Associate II
  • 1847 Views
  • 2 replies
  • 0 kudos

SPI Software Chip Select

Posted on February 14, 2015 at 13:46 What is the best way to implement chip select in software? I've tried doing it this way: HAL_GPIO_WritePin(NSS_PORT, NSS_PIN, GPIO_PIN_RESET); HAL_SPI_Transmit(&hspi1, out , 1); HAL_GPIO_WritePin(NSS_P...

dscdsc by Senior
  • 3327 Views
  • 5 replies
  • 0 kudos

Update Binary with Bootloader

Posted on February 23, 2015 at 16:29Hello,I´m trying to update my application with the Preprogramed bootloader by apropiate uart and pins BOOT1/0 according to that task.I could use this application to do that, couldnt I?My Keil compilation makes 2 f...

0690X000006030NQAQ.jpg 0690X000006030SQAQ.jpg
gerardo by Associate II
  • 1535 Views
  • 2 replies
  • 0 kudos

Poblem programming stm32f334 witn the flash loader demo 2.7.0

Posted on February 19, 2015 at 09:09I can program the stmf32f334 chip without problem with the  desktop version ''FlashLoaderDemo.2.7.0'' - it is Ok. But the command line version gives error: ''The instruction of ''0x7c911699'' referenced memory of ...

var2 by Associate III
  • 1885 Views
  • 3 replies
  • 0 kudos

5 V pulse board stm32f407

Posted on February 19, 2015 at 16:28Hello, i want to generate a periodic pulse of 5V into a pin using a TIMER. Has someone a code similar to this? Thank you #timers #stm32f4 #stm32f407 #discovery

fiulala by Associate II
  • 1294 Views
  • 2 replies
  • 0 kudos

Will STM32F407ZG supports using AS1115 driver ?

Posted on February 23, 2015 at 10:33I am having a custom board with STM32407ZG, the board also has AS1115 driver IC for supporting the keypad and led lights. Is there any example relating to this combo? #stm32f407zg #- #as1115 #example

dhinesh by Associate
  • 981 Views
  • 1 replies
  • 0 kudos

Hard Fault-> INVALID STATE when calling WFI() STM32L

Posted on July 31, 2014 at 10:46I hit an issue with our STM32L project that is giving meheadaches.We have recently upgraded from STM32L151VB to STM32L151VC as we needed the extra RAM.Migrating the code though, has started triggering HARDfaults with ...

0690X000006051eQAA.png
ioannis2 by Associate II
  • 7980 Views
  • 14 replies
  • 0 kudos

interrupt driven usart2 reception not working

Posted on February 16, 2015 at 03:11Hi,This is kiran kadam.currently i am working on gsm based project.tools i am using for development are stm32f429 disco board,sim900 module,level converter and ewarm7.3i am stuck at interrupt driven uart.i have wr...

kiran2 by Associate II
  • 4684 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.