STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Communication between two STM32F4 DISCOVERY boards

Posted on February 22, 2015 at 17:49Hi, I'm currently trying to send data from one STM32F4 board as a master to the other STM32F4 board which is the slave via SPI. However recever data are incorect.//************************Code Master**************...

Difference between HSE and HSE Bypass

Posted on February 21, 2015 at 17:51After some hardware struggles with my new STM32F3 disco board I finally got it running correctly and at high speed. I was wondering, however, that there seems to be no difference between HSE and HSE bypass mode, a...

How to determine the origin of Wakeup from Standby?

Posted on February 16, 2015 at 21:41I am studying awakening from Standby Mode on STM32F100CB. I have this context: we set up WKUP pin and RTC Alarm, and go to Standby. Then, rising edge on WKUP pin or RTC Alarm wakes the system up. Here are a few th...

apolotsk by Associate II
  • 1599 Views
  • 4 replies
  • 0 kudos

STM32F205RCTb system boot loader

Posted on February 18, 2015 at 10:52HiWe want to use USB DFU feature available in system bootloader for firmware upgradeController used: STM32F205RCTbHow to jump to bootloader from application(Running in Flash). what should be the Boot options (Boot...

sangamesh by Associate II
  • 1348 Views
  • 3 replies
  • 0 kudos

Timer 3 PWM - strange behaviour on first pulse

Posted on February 18, 2015 at 23:50Hello, I am programming Timer 3 for PWM mode. Please see the attached image. The yellow trace is Timer 3, the green is Timer 4, which follows Timer 3 by a period of 180 degrees shift. The top PWM train (Timer 3) ...

How can put points between the string?

Posted on February 20, 2015 at 02:05 hi all How can put points between the string? ( for example: 00.00) thanks void Str_convert(unsigned long t, unsigned char *str, unsigned char n) { unsigned ...

kemal by Associate II
  • 1154 Views
  • 2 replies
  • 0 kudos

DAC can't output 0V

Posted on February 19, 2015 at 07:41 I'm using stm32f429 discovery board. I have configured DAC Channel 1 (PA4) for DAC ouput. When I try to configure ouput in the range of 0.15v - Vref(2.97v) I'm getting the ouput properly, but when trying to ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.