STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hard Fault-> INVALID STATE when calling WFI() STM32L

Posted on July 31, 2014 at 10:46I hit an issue with our STM32L project that is giving meheadaches.We have recently upgraded from STM32L151VB to STM32L151VC as we needed the extra RAM.Migrating the code though, has started triggering HARDfaults with ...

0690X000006051eQAA.png
ioannis2 by Associate II
  • 7840 Views
  • 14 replies
  • 0 kudos

interrupt driven usart2 reception not working

Posted on February 16, 2015 at 03:11Hi,This is kiran kadam.currently i am working on gsm based project.tools i am using for development are stm32f429 disco board,sim900 module,level converter and ewarm7.3i am stuck at interrupt driven uart.i have wr...

kiran2 by Associate II
  • 4576 Views
  • 11 replies
  • 0 kudos

TIM2 Interrupt period issue

Posted on February 22, 2015 at 21:49The original post was too long to process during our migration. Please click on the attachment to read the original post.

SPI Communication between two STM32F4 DISCOVERY boards

Posted on February 22, 2015 at 17:49Hi, I'm currently trying to send data from one STM32F4 board as a master to the other STM32F4 board which is the slave via SPI. However recever data are incorect.//************************Code Master**************...

Difference between HSE and HSE Bypass

Posted on February 21, 2015 at 17:51After some hardware struggles with my new STM32F3 disco board I finally got it running correctly and at high speed. I was wondering, however, that there seems to be no difference between HSE and HSE bypass mode, a...

How to determine the origin of Wakeup from Standby?

Posted on February 16, 2015 at 21:41I am studying awakening from Standby Mode on STM32F100CB. I have this context: we set up WKUP pin and RTC Alarm, and go to Standby. Then, rising edge on WKUP pin or RTC Alarm wakes the system up. Here are a few th...

apolotsk by Associate II
  • 1554 Views
  • 4 replies
  • 0 kudos

STM32F205RCTb system boot loader

Posted on February 18, 2015 at 10:52HiWe want to use USB DFU feature available in system bootloader for firmware upgradeController used: STM32F205RCTbHow to jump to bootloader from application(Running in Flash). what should be the Boot options (Boot...

sangamesh by Associate II
  • 1311 Views
  • 3 replies
  • 0 kudos