STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeF4: EEPROM emulation

Posted on March 20, 2014 at 06:11Is there EEPROM emulation in STM32CubeF4?Page http://www.st.com/web/en/catalog/tools/PF257902 has status NRND and recommends use  STM32CubeF4, but I don't see EEPROM emulation in those bibls

pestov by Associate III
  • 3353 Views
  • 10 replies
  • 0 kudos

STM32F4 Discovery TCP problem

Posted on March 02, 2015 at 11:20Hello, I am trying to implmenet TCP server on my STM32F4 Dis which connects to a client computer via Ethernet. The Client computer keeps sending connection request and data to the server and receives the data from th...

USB Host stack is not stable during CDC communication

Posted on February 04, 2015 at 21:20Currently we are working with STM32F217 MCU and we use USB Host in FS mode to communicate with some external device. We use CDC class driver generated by STM32Cube plug-in to Eclipse. We are facing some problems w...

lukasz23 by Associate II
  • 2882 Views
  • 7 replies
  • 0 kudos

GUI Builder

Posted on March 04, 2015 at 08:03Have someone used ST GUI Lib together with displays of 800x480? When I start GUI builder, and select this resolution only a part of my new screen is shown. Does anyone have any idea?? Have someone used this Lib with ...

oe2 by Associate III
  • 948 Views
  • 1 replies
  • 0 kudos

I2C Issues Using STM32F429I Discovery Board.

Posted on February 13, 2015 at 13:23 I am attempting to configure the pins on the STM32F429I Discovery Board so that i can connect some I2C sensors and produce some data readings for a project i am working on. I am using the template file gi...

mw876 by Associate
  • 1207 Views
  • 1 replies
  • 0 kudos

Need help with STM32F072 timer 3 output compare unit

Posted on March 03, 2015 at 19:06Hello. Thanks for helping.  I have a need to generate fairly precise output pulses atsomewhat irregular intervals.  I have timer 3, Ch1 set up forinput capture, and it works great. I have the timer set to roll overat...

lou by Associate II
  • 2951 Views
  • 6 replies
  • 0 kudos

PGERR writing user data option bytes STM32F103RE

Posted on March 03, 2015 at 18:44Hi all,I am trying to read and write the STM32F103 user data bytes (Data0 and Data1 in Table 8 of STM32F10xxx PM0075 Programming manual).I wrote this code to set Data0 to value 0x1B:  FLASH_UnlockBank1();            ...

okelly by Associate II
  • 2313 Views
  • 3 replies
  • 0 kudos