STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX Clock Configuration Problem

Posted on March 04, 2015 at 23:44 I'm trying to use Cube for an STM32F042 project and I'd like the APB1 peripheral clock to be 1 MHz but Cube is saying that the minimum APB1 peripheral clock is 10 MHz. Is this true or is this a problem with Cube? ...

SMT32F4 Discovery - VCP+I2C problem

Posted on March 02, 2015 at 16:06Hi, I'm using an STM32F4 Discovery board. I need to send some coefficients from a PC via putty to a digital audio processor (with which I communicate via I2C). I would like to use either one of the USB ports on the b...

STM32L0: Problem with adc multichannel

Posted on March 04, 2015 at 15:18Hello, I want to read several voltages with the adc of the STM32L051K8. If I convert only one channel, then the value is correct, but if it convert several channel is has an incomprehensible behavior. Sometimes it sa...

danilo23 by Associate
  • 1269 Views
  • 2 replies
  • 0 kudos

ADC reading 15% low on one channel

Posted on March 03, 2015 at 21:57I am using the STM32F429IIH6 for a project.I have 3 ADC channels.  Two are working properly, but one is consistently reading 15% low (compared to a DMM).  PC2 is the pin not working properly.e.g., when I read the ADC...

How to start 2 timers at the same time

Posted on March 04, 2015 at 13:59Hello, is it possible to start 2 timers exactly at the same time? If I enable first timer and then enable the second timer, it takes some time... Thank you for answeres and ideas.

j3lda by Associate II
  • 1499 Views
  • 1 replies
  • 0 kudos

Using emmc and fatfs with STM32F207

Posted on March 04, 2015 at 11:01Dears, I plan tu use an eMMC memory chip with an STMF32f207 connected to the SDIO interface (4-bits wide) and an FAT lib (from ST). The eMMC choice is dictated by wear levelling and ECC management facilities. All the...

STM32CubeF4: EEPROM emulation

Posted on March 20, 2014 at 06:11Is there EEPROM emulation in STM32CubeF4?Page http://www.st.com/web/en/catalog/tools/PF257902 has status NRND and recommends use  STM32CubeF4, but I don't see EEPROM emulation in those bibls

pestov by Associate III
  • 3347 Views
  • 10 replies
  • 0 kudos