STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART2 interrupt continuosly fires

Posted on March 11, 2015 at 14:55Hello all,I have a problem with my USART2 interrupt on STM32L151.I have the USART_IT_RXNE, and USART_IT_TXE interrupts enabled on UART2. All other interrupts are disabled. The interrupt works fine until something wei...

srdjan by Associate II
  • 3279 Views
  • 11 replies
  • 0 kudos

my ADC code cann't get value

Posted on March 04, 2015 at 17:41The original post was too long to process during our migration. Please click on the attachment to read the original post.

LWIP ETHERNET PROBLEM

Posted on March 11, 2015 at 13:43hii used lwip example in stm32cubef4 like to(udp echo server,tcp echo server,......).when i connect 2 stm32f407 eval boards as udp or tcp servers to ethernet hub switch and connect to pc as client my servers don't wo...

osMailQDef error in cmsis_os.h

Posted on March 10, 2015 at 19:09The definition of the osMailQDef macro is incorrect in cmsis_os.h; it is missing a semicolon. Here is the original version: #if defined (osObjectsExternal)  // object is external #define osMailQDef(name, queue_sz, ty...

ccox by Associate II
  • 1137 Views
  • 1 replies
  • 0 kudos

Upgrading STM32F429 firmware using a USB key

Posted on March 29, 2014 at 19:13Dear All,I would like to upgrade / update the STM32F429 firmware using a USB Key.I have found one application note, but I have not found any working example.Does anyone have some working example or some advise?Let me...

STM32L1 & linear CMOS image sensor

Posted on March 11, 2015 at 13:20 Hi everyone, I am trying to interface a linear CMOS image sensor by Hamamatsu (S9226-03) with a STM32L1 discovery board, and seek a bit of guidance on how exactly to accomplish that in a suitable way, since I...

o23 by Associate
  • 1266 Views
  • 0 replies
  • 0 kudos

Has anyone ported LwIP 1.4.1 to CMSIS-RTOS/RTX

Posted on December 19, 2014 at 22:48Hi,I am new to programming ST microcontrollers, and I am trying to get a demo tcpecho application running on my custom hardware.  We are using an STM32F407.  I notice that all the examples seem to use FreeRTOS and...

separating bitmaps from code

Posted on March 10, 2015 at 11:21Hi All,I'm on the tail end of a large development for an stm32 using gcc and openocd. As I add more code and bitmaps (for the LCD) I'm finding the load times getting rather long, mainly due to the bitmaps.I'd therefo...

mark2399 by Associate II
  • 1913 Views
  • 4 replies
  • 0 kudos

How to detect MCU at run time?

Posted on March 10, 2015 at 14:57Hi,Is there a way to determine which MCU is being used on a board?  We are developing software for an STM32F4 and some of our tools are using the 407 and others are using a 429.  I would like to know when our code is...