cancel
Showing results for 
Search instead for 
Did you mean: 

Double buffered DMA Interrupt not working

bmentink
Associate II
Posted on August 02, 2014 at 10:01

Hi All,

New to the STM32 so please bare with me....

I have setup timer4 to generate a sinewave modulated PWM using double buffered DMA and that works very well, I can see my waveform on the pin and it contains the correct data from each of the two buffers.

However, I am trying to update the buffers via the half completed interrupt and I don't seem to be getting any action at all ...

The code that sets up the DMA and the interrupt and the interrupt routine itself follows:

-------------------------------------------------------------------

void DMA_Configuration(void)

{

  DMA_InitTypeDef DMA_InitStruct;

  NVIC_InitTypeDef NVIC_InitStructure;

 

  // TIM4_UP - DMA1, Channel 2, Stream 6

 

  DMA_InitStruct.DMA_Channel            = DMA_Channel_2;

  DMA_InitStruct.DMA_BufferSize         = PWM_ELEMENTS;

  DMA_InitStruct.DMA_DIR                = DMA_DIR_MemoryToPeripheral;

  DMA_InitStruct.DMA_Mode               = DMA_Mode_Circular;

  DMA_InitStruct.DMA_FIFOMode           = DMA_FIFOMode_Disable;

  DMA_InitStruct.DMA_FIFOThreshold      = DMA_FIFOThreshold_HalfFull;

  DMA_InitStruct.DMA_Memory0BaseAddr    = (uint32_t)&PWM_Buffer[0];

  DMA_InitStruct.DMA_MemoryBurst        = DMA_MemoryBurst_Single;

  DMA_InitStruct.DMA_MemoryDataSize     = DMA_MemoryDataSize_HalfWord;

  DMA_InitStruct.DMA_MemoryInc          = DMA_MemoryInc_Enable;

  DMA_InitStruct.DMA_PeripheralBaseAddr = (uint32_t)&TIM4->CCR1;

  DMA_InitStruct.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

  DMA_InitStruct.DMA_PeripheralInc      = DMA_PeripheralInc_Disable;

  DMA_InitStruct.DMA_Priority           = DMA_Priority_Medium;

 

  DMA_Init(DMA1_Stream6, &DMA_InitStruct);

  // Disable stream

  DMA_Cmd(DMA1_Stream6, DISABLE);

  // Configure double DMA mode.

  // This function can be called only when the DMA Stream is disabled.

  DMA_DoubleBufferModeConfig(DMA1_Stream6,(uint32_t)&PWM_Buffer2[0],DMA_Memory_0);

  // Enable DMA double mode. This function can be called only when the DMA Stream is disabled.

  DMA_DoubleBufferModeCmd(DMA1_Stream6, ENABLE);

  //!Enable DMA transfer complete interrupt

  DMA_ITConfig(DMA1_Stream6, DMA_IT_TC, ENABLE);

  NVIC_InitStructure.NVIC_IRQChannel = DMA1_Stream6_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

  NVIC_EnableIRQ(DMA1_Stream6_IRQn);

  // turning DMA on

  DMA_Cmd(DMA1_Stream6, ENABLE);

}

// Interrupt handler for dma transfer 1/2 finished, i.e after one buffer done.

void DMA1_Stream6_IRQHandler(void) {

    // Stream6 transfer complete interrupt?

    if(DMA_GetITStatus(DMA1_Stream6, DMA_IT_TCIF6)) {     // Transfer Complete event

        // clear pending interrupt

        DMA_ClearITPendingBit(DMA1_Stream6, DMA_IT_TCIF6);

        if(DMA_GetCurrentMemoryTarget(DMA1_Stream6)) {

        }

        else{

        }

    }

}

-----------------------------------------------------------------

Can anyone help?

EDIT: This is on a STM32F4Discovery Board

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 02, 2014 at 22:08

Using a C++ compiler?

Does the handler show up in the .MAP file, and do you have linkage to it through the vector table?
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
bmentink
Associate II
Posted on August 02, 2014 at 22:33

Hi Clive,

No it is not in the .map file, how do I link it for this processor? That name is in the vector table, I just thought you had to define it?

Cheers,

Bernie