STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIM17 PWM

Posted on July 19, 2011 at 17:47Hi, I am trying to produce PWM signal by using TIM17 channel1 on PORTB-9, but i can't get the PWM signal. In debug mode i can see that TIM17 COUNTER register advanced and do overloop, but i just cant see the PWM signa...

ybitton by Associate II
  • 1713 Views
  • 3 replies
  • 0 kudos

Filtered data value is so long

Posted on May 25, 2015 at 08:16I am using stm32f4 discovery board. from ADC I take 1ksample/sec and accumulate it. after accumulation of 30Ksamples, process it through band pass filter. output of band pass filter is very large +ve and -ve values ex...

lokesh by Associate II
  • 3641 Views
  • 8 replies
  • 0 kudos

debugging STM32 : need some newbie suggestions

Posted on May 28, 2015 at 10:37In a few days I will start the first project with STM32 on a dedicated hardware. I would like to ask some suggestions about debugging: 1) JTAG or SWD? So far I used JTAG on AVR core and it worked fine. I don't know SWD...

infor by Associate III
  • 1212 Views
  • 2 replies
  • 0 kudos

Problem with STM32F401 OTG FS MSC using SDIO uSD card

Posted on May 26, 2015 at 21:23Hi, all. I have an STM32F401Discovery Kit using an STM32F401VCT6. I have wired an external SD card connector and have successfully implemented Elm-Chan's FATFs using the SDIO SD card interface. All works well, I can mo...

STM32427 with CubeMX

Posted on May 23, 2015 at 11:34I have a board with a 32 bit SRAM and have used CubeMX to configure a 32 bit data bus, a 10 bit Address bus with a Chip select of NE1. Briefly, Cube has produced the MX_FMC_Init(); file with settings as follows:- hsram...

NVIC_ISPR ''set-pending'' bit to force ISR entry

Posted on May 25, 2015 at 03:50 Hi, I'm running some tests on an STM32F072 to verify my understanding of the docs. Apparently I'm missing an important point regarding the NVIC and pending interrupts... I'm single-stepping through the code ...

fenugrec by Associate II
  • 2596 Views
  • 3 replies
  • 0 kudos

CMSIS: DSP Lib - Frequency Bin Example

Posted on May 22, 2015 at 16:18Estimated colleagues, following I explain the strange behavior:     I am working the STM32F407 ARM processor,    compiling with the GNU Tools ARM (4_9-2014q4) ,    use the HAL provided by STM32CubeF4 v1.5.0,    using...

rs2 by Associate II
  • 3601 Views
  • 4 replies
  • 0 kudos

Need help to execute program from SRAM

Posted on May 21, 2015 at 12:39Hi, I want to execute my code from SRAM of STM32F100. I basically want to copy a program from flash to SRAM and execute the program from SRAMPlease help me understand how this can be addressed.Regards Tejas #flash #...

tejas by Associate II
  • 1918 Views
  • 3 replies
  • 0 kudos