Question
CAN Loopback scoped Tx dead
Posted on November 12, 2014 at 12:04
Hi!
I am using a DevKit407 ( stm32f4 discovery + stm32f4dis-BB).- I managed to set up a perfectly functioning
CAN1 in Loopback mode
. I assume I should see the test frame sent on Tx pin (PB9 on stm32f4discovery, or CAN1_TX on BB) with an oscilloscope (sampling rate 2.5 GS/s) .But I do not see any movement.
Internally shorting the Tx/Rx pins will close Tx pin? - Is there a problem if I use split termination, but the connected devices will have simple 120 Ohm termination?
Thank you for your time and knowledge!
#discovery #can #stm32f4