cancel
Showing results for 
Search instead for 
Did you mean: 

Pending TIM bits

Valeev.Kamil
Associate II
Posted on December 12, 2014 at 08:57

Hello forum,

I have a weird issue with TIM's pending bits (I mean Cortex-M3 pending bits): they are set after enabling the overflow interrupt:

void InitTIM4() {

  TIM_TimeBaseInitTypeDef timer;

  TIM_TimeBaseStructInit(&timer);

  timer.TIM_CounterMode = TIM_CounterMode_Up;

  timer.TIM_Prescaler = 9;

  timer.TIM_Period = 79;

  TIM_TimeBaseInit(TIM4, &timer);

  TIM_Cmd(TIM4, ENABLE);

  TIM_ITConfig(TIM4, TIM_IT_Update, ENABLE);

}

Therefore after enabling all interrupts with __enable_irq (), program goes to corresponding Handlers immediately, although it should go there after TIM overflows. I tried clearing pending bits with NVIC_ClearPendingIRQ() but it didn't work. Maybe i'm not understanding or missing something simple, i don't know.

I'm using STM32F100RB MCU.

Sorry for my poor English.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Valeev.Kamil
Associate II
Posted on December 12, 2014 at 11:30

Nevermind. I didnt clear request interrupt AND pending interrupt after the TIM4->EGR |= TIM_EGR_UG