Skip to main content
roy23
Associate II
December 12, 2014
Question

STM32F0 - SPI 8bit data size

  • December 12, 2014
  • 0 replies
  • 689 views
Posted on December 12, 2014 at 08:53

I am migrating code from STM3210x to STM32F0xx. major part of the application uses spi interface. I see in logic analyzer each bursts of 16bit clocks. while I expect it to be 8bit clock for each byte and a delay of one byte between the clocks. I am attaching the signals.

inside attachments you can so how its initialized and the outcome. 

Can someone suggest  how to get the same signaling in STM32F0 to be like the STM32F10 ?

I have tried using SPI_Senddata8, change the  SPI_InitStructure.SPI_DataSize with no success.

The code I am using is as folow:

   SPIx_CS_GPIO->BRR = SPIx_CS;

    for(i=0; i<headerLength; i++)

    {

     SPIx->DR = headerBuffer[i];

      while((SPIx->SR & SPI_I2S_FLAG_RXNE) == (uint16_t)RESET);

      temp = SPIx->DR ;

    }

    for(i=0; i<readlength; i++)

    {

     SPIx->DR = 0;

     while((SPIx->SR & SPI_I2S_FLAG_RXNE) == (uint16_t)RESET);

    readBuffer[i] = SPIx->DR ;//port_SPIx_receive_data(); //this clears RXNE bit

    }

    SPIx_CS_GPIO->BSRR = SPIx_CS;

Thanks,

Roy

#stm32f0
This topic has been closed for replies.