STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I²S on STM32F411

Posted on June 30, 2015 at 15:49 Hi! I'm trying to communicate with a http://www.cirrus.com/en/pubs/proDatasheet/CS4344-45-48_F2.pdfDAC via I²S but I can't get it to work. I followed the steps on the STM32's HAL http://www.st.com/st-...

florent2 by Associate II
  • 1017 Views
  • 1 replies
  • 0 kudos

stm32f4_extenal_clock

Posted on June 29, 2015 at 13:28hello every one i use stm32f429 micro controller and use external 8mhz oscillator as external clock src. and connect output frq of the oscillator to osc_in pin  and osc_out is floating. every thing work correctly i us...

STM32f0 ADC_IT_EOC is not getting set

Posted on June 30, 2015 at 12:33Hi All,           Iam using stm32f051r8t6 discovery for my application,facing problem while debugging the code in KEIL using stlink. The problem is when I enable ADC_IT_EOC though the ADC1_COMP_IRQHandler is getting i...

surya by Associate
  • 820 Views
  • 0 replies
  • 0 kudos

SPI clock initialisation problem

Posted on June 30, 2015 at 10:05 Hi everybody, I have a problem while doing the configuration of the SPI on my stm32f051r8. Indeed, I've written the hole initialization code but I can't see the the clock with a scope.. Can you help me? ...

2 PWM with phase shift

Posted on June 28, 2015 at 17:36Hi, I would like to generate 2 PWM @ 6KHz, but i would like to have a delay between the PWMs of 5uS. I thought of using two different timers for the mission (each for each PWM), and just for the first time delay to us...

udibit by Associate II
  • 1688 Views
  • 3 replies
  • 0 kudos

float numbers in IEEE 754

Posted on June 29, 2015 at 09:37Hello Sirs,Doesanybody use IEEE 754 format to represent float numbers?I need toconvert values to this standard format, and I was wondering if someone of youhas already done it with any STM32F.  I�d bepleased if you ca...

STM32 I2C reading more than 2 bytes

Posted on June 29, 2015 at 16:37 Hi I'm trying to get a STM32F427 working as a I2C master using interrupts and everything is working apart from reading more than 2 bytes. I can write any number of bytes and read 1 or 2 bytes all OK. ...

Timer Synchronization with Offset

Posted on June 29, 2015 at 20:43Hello everyone, Excuse me for creating a discussion similar to one that I have already created, but I decided to give it a last try, because I could really use some help. What I want to do precisely is this: Timer1 (P...

pant by Associate II
  • 1172 Views
  • 0 replies
  • 0 kudos