STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI1 hardware NSS output ?

Posted on October 04, 2015 at 12:58 Guys, How can I control SPI1 hardware NSS output (PA4) ? I tried to give a signal to it, but nothing on my logic analyzer... #define Mp3SelectControl() { HAL_GPIO_WritePin(GPIOA, GPIO_PI...

Error in the F7 DISCO Documentation

Posted on October 05, 2015 at 14:50There is a very nasty error in the UM1907 - the net labels ARD_D5 and ARD_D10 are connected to PI.10 and PA.8 on the schematic on page 32 but on the schematic on page 29 AND in the table on page 19 the labels and ...

cm600 by Associate II
  • 877 Views
  • 1 replies
  • 0 kudos

STM32F105RC UART problem

Posted on October 05, 2015 at 03:26 Hi, I'm currently working with STM32F105RC chip and trying to use UART4 (PC10 and PC11), which connects to a USB to UART module to a computer. The problem is, I'm not getting any readings from PC using hyperte...

IAP for STM32F4 Discovery

Posted on September 11, 2013 at 09:34Hello,Is it possible to use the IAP example which is referred in an3965 directly in the STM32F4 Discovery board? Thank you. #stm32f4 #discovery #iap #iap #wait-for-you--clive1-!-!-!

pradeepa by Associate II
  • 4094 Views
  • 9 replies
  • 0 kudos

STM32L4 Ultra-Low-Power MCU Google Hangout Tomorrow

Posted on September 30, 2015 at 22:00Not sure it was mentioned here, but just an FYI. It's done in the morning in the North American territory, so should be reachable by the European audience late afternoon.Google Hangout ''Getting started with STM3...

RTC week day

Posted on October 03, 2015 at 21:33Hello,I'm working on a STM32L053 and I have a question about RTC and ''week day''. When I provide a date: YYYY-MM-YY  without day of week, I would like to know if the STM32L053 RTC hardware can calculate the week d...

purkovic by Associate II
  • 2706 Views
  • 3 replies
  • 0 kudos

stm32f4 IAP-how to produce a bin file for IAP programme

Posted on October 04, 2015 at 04:00Hello,I'm using stm32f4 discovery board. The IDE I'm using is IAR EWARM. I have tried the sample code for IAP. But i want load my own code/program into the flash memory. So how i can produce a bin file which can be...