cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the datasheet? OR Where is my tutorial?

monomonster
Associate II
Posted on April 29, 2015 at 14:24

I bought a discovery board with STM32F4 family processor (comes with a TFT LCD). I have my IDE working and downloaded CubeMX and generated some init code - no problem.

Now, I don't know how to do anything! How do I toggle a pin? How do I use the peripherals? Where is all that sort of data written?

I went through all the files in the discovery board page and nothing really helpful in there. The only thing I have managed to understand is that CubeF4 is contains libraries and drivers that I can use to simplify development. But is there any text on these? A datasheet of some sorts that also explains a bit about the architecture?

#discovery #stm23f4 #getting-started
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on April 29, 2015 at 14:33

Data for chip, and design support information.

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1577/LN1806/PF255419

I'd recommend the Standard Peripheral Library over Cube

http://www.st.com/web/en/catalog/tools/PF257901

And the firmware examples for the STM32F429I-DISCO

http://www.st.com/web/en/catalog/tools/PF259429

Ignore the Cube messaging, go to the Red Download buttons at the bottom of the pages.

Should be a Windows Help file in the root directory of one of the packages.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..