STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 Ultra-Low-Power MCU Google Hangout Tomorrow

Posted on September 30, 2015 at 22:00Not sure it was mentioned here, but just an FYI. It's done in the morning in the North American territory, so should be reachable by the European audience late afternoon.Google Hangout ''Getting started with STM3...

RTC week day

Posted on October 03, 2015 at 21:33Hello,I'm working on a STM32L053 and I have a question about RTC and ''week day''. When I provide a date: YYYY-MM-YY  without day of week, I would like to know if the STM32L053 RTC hardware can calculate the week d...

purkovic by Associate II
  • 2718 Views
  • 3 replies
  • 0 kudos

stm32f4 IAP-how to produce a bin file for IAP programme

Posted on October 04, 2015 at 04:00Hello,I'm using stm32f4 discovery board. The IDE I'm using is IAR EWARM. I have tried the sample code for IAP. But i want load my own code/program into the flash memory. So how i can produce a bin file which can be...

STM32 F0 Discovery - interrupt question

Posted on October 04, 2015 at 00:20 I am CubeFX and Keil. Hardware is Discovery board with STM32F051R8T6. Created an interrupt for PA0 (user button) and toggle an led (PC9 green LED). This works void EXTI0_1_IRQHandler(void) { i...

irslabs by Associate
  • 822 Views
  • 1 replies
  • 0 kudos

STM32F4 USART PROBLEM

Posted on October 02, 2015 at 23:18Hi guys, I have a problem. I have a USB-RS232 converter and i'll do usart tutorial with STM32F4. Codes are working, but meaningless character viewing at the serial Hyper terminal program. Baudrate 9600. Clock Confi...

STM32F4 DISCO data transfer

Posted on September 30, 2015 at 15:31I want to pass data from MP45DT02 MEMS mic  to the audio DAC CS43l22. All the configurations seems okay, the thing I can't seem to achieve is the correct Fifo buffer. The FIFO read variable (which points to the n...

matas by Associate II
  • 1619 Views
  • 3 replies
  • 0 kudos

Lwip tcp stack is locking after 2-3 days of working

Posted on September 02, 2015 at 15:20LWIP stack is lockingup about every 48-60 hours, with a casually polling ModbusTCP connection (~ 1000 ms between polls).It requires apower cycle of our equipment to restore the operation of the stack.i use codes ...

mustafa23 by Associate II
  • 2777 Views
  • 5 replies
  • 0 kudos

STM32F105RC UART problem

Posted on October 03, 2015 at 04:20 Hi, I'm currently working with STM32F105RC chip and trying to use UART4 (PC10 and PC11), which connects to a USB to UART module to a computer. The problem is, I'm not getting any readings from PC using hyperte...

Possible to Trigger SPI DMA Transfer from Timer?

Posted on August 22, 2015 at 07:04I am using an STM32F407 chip on a custom PCB. Using (mostly) HAL libraries, but I've ended up writing a lot of my code and verifying the registers individually. I am using an ADC that communicates over SPI. The tran...

ravix475 by Associate II
  • 2431 Views
  • 3 replies
  • 0 kudos

STMCube and SPL

Posted on January 23, 2015 at 11:26having developed with the SPL in the past, and now tried the STMCube i would like to make a couple of observation. - i understand the rational for the development of the STMcube tool, but it is forcing developers d...

caspar by Associate
  • 6571 Views
  • 13 replies
  • 1 kudos