STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Driving an LCD - FSMC vs FMC vs LTDC

Posted on October 08, 2015 at 13:32I must select a MCU for a project which should use a TFT LCD (240x320). I would like to know what are the main differences between FSMC, FMC and LTDC interfaces for driving an LCD. If FSMC is OK then the value line...

e1369008 by Associate II
  • 3128 Views
  • 3 replies
  • 0 kudos

Bug Comment of HAL-DMA Lib

Posted on October 08, 2015 at 13:18Hi, in this part of the DMA-SetConfig() function the comments are wrong. /* Memory to Peripheral*/   if((hdma->Init.Direction) == DMA_MEMORY_TO_PERIPH)   {     /* Configure DMA Stream destination address */     hdm...

ADC triple Injected mode in stm32f4discovery

Posted on October 08, 2015 at 18:29Hello,   I have been trying for days to get the ADC in STm32f4Discovery board to work in triple regular Injected simultaneous mode with no luck. My intended goal is setup the ADC to work in triple Injected simultan...

Nucleo board USB and SDIO signal integrity

Posted on August 25, 2015 at 20:45I am thinking of building several ''shields'' with GSM, GPS, LCD, MicroUSB and MicroSD connectors to stack up on the STM32F401 Nucleo board (by the dual row connectors, not Arduino) but i'm worried about the signal ...

STM32f4 different timers

Posted on October 08, 2015 at 17:35 Hi, I'm working with stm32f4-disco. I made a code that works well: the micro waits for an external interrupt, and when receives the interrupt it makes pulses of 40kHz with a duration of 1 ms. Now, I wanted...

fiulala by Associate II
  • 1604 Views
  • 3 replies
  • 0 kudos

Incorrect baudrate with STM32F103 and Smartcard on USART2

Posted on October 07, 2015 at 15:53Hi all, I am using a STM32F103 chip where USART1 and USART2 are connected to Smartcard units. I have tried to communicate to the Smartcard by first sending a reset signal (according to ISO 77816 definition) and the...

danesh by Associate II
  • 1291 Views
  • 2 replies
  • 0 kudos

STM32Cube L4 demos

Posted on October 02, 2015 at 22:06Hi there. Thanks for the STM32Cube software.  I have a Discovery board and would like to try some USB-OTG testing, but there are only USB demo apps for the EVAL board, is it possible to port them so they run on the...

Is this a bug? - STM32L4, HAL, USART DMA handler

Posted on October 02, 2015 at 14:39Using HAL, I have configured DMA1_CH2 and USART3_TX such that once in a while, a block of bytes will be copied from memory to peripheral, in NORMAL, i.e. non-circular mode. Now, my handler, HAL_USART_TxCpltCallback...

8 bits DAC DMA config on STM32F2

Posted on October 04, 2015 at 17:07 Hi all, I am not sure about a DMA config for DAC on STM32F2. Could you please tell me if I made an error using 8bits words with this DMA config? Especially with DAC base address? #define BUFF...

neoirto by Associate II
  • 2062 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.