2015-04-20 3:57 PM
Hi, I made a custom board to atach to a nucleo 411 board with a uSD shocket. I'm trying to get FatFs on it. I'v test almost every code on the web. I use System Workbench and Cube/stdperiph_lib.
I would like a simple initialization and test software just to dichard hardware problem. I'v saw a lot of examples, but with DMA and other things. Is there a simple example just to test the minimun necesary comunication with the SD ? jus to be sure that there is no hardware issue on my board. Thank!2015-04-20 7:22 PM
Well, I make a simple cube mx project, just with SDIO config.
I obtain this into main.cint main(void)
{
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_SDIO_SD_Init();
while (1)
{
}
/* USER CODE END 3 */
}
I debug it and step by step go into
MX_SDIO_SD_Init
void MX_SDIO_SD_Init(void)
{
hsd.Instance = SDIO;
hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
hsd.Init.ClockDiv = 0;
HAL_SD_Init(&hsd, &SDCardInfo);
}
I don't go into HAL_SD_Init, I just wait until it execute, and then I saw what SDCardInfo have:
https://www.dropbox.com/s/jgrm9w380sqwyf2/Captura%20de%20pantalla%202015-04-20%png?dl=0
So I can see info about my SD card, and it seems to be ok (CardCapacity is almost 1Gb)
So may I say that my hardware is ok? or I need to run some other test? If I can't make FatFs working is becouse a software problem?
Thank
2015-04-20 7:43 PM
Now I add this code on main.c:
err = HAL_SD_ReadBlocks(&hsd, buf, 0, 512, 4);
And I obtain this into buf:
Name : buf
Details:''ë<\220MSDOS5.0\0\002 \002\0\002\0\002\0\0øç\0?\0ÿ\0\0\0\0\0\0À\034\0\0\0)Ë\214ÎtNO NA
E FAT16 3É\216Ѽð{\216Ù¸\0 \216Àü½\0|8N$}$\213�?\231è<\001r\034\203ë:f¡\034|&f;\a&\212Wüu\006\200Ê\002\210\026\002\200Ã\020së3É\212F\020\230÷f\024\003F\034\023V\036\003F\016\023Ñ\213v\021`\211Fü\211Vþ¸ \0÷æ\213^\v\003ÃH÷ó\001Fü\021Nþa¿\0\0èæ\0r9&8-t\027`±\v¾¡}ó¦at2Nt\t\203Ç''...
Default:0x20000460
Decimal:536872032
Hex:0x20000460
Binary:100000000000000000010001100000
Octal:04000002140
So, the hardware is Ok, right?
2015-04-21 6:08 AM
Hi,
How did you made the connection (pin numbers -> SD)? Did you use pull-up resistors?2015-04-21 8:47 AM
I use PC8, PC12 and PD2, this is ok. I have PU resistor on CMD and D0 lines
I test this code:/* Includes ------------------------------------------------------------------*/
#include ''stm32f4xx_hal.h''
#include ''stm32f4xx_hal_sd.h''
#include ''sdio.h''
#include ''gpio.h''
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static uint32_t buf[512*4];
int main(void)
{
HAL_SD_ErrorTypedef err;
uint32_t cnt=0;
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_SDIO_SD_Init();
while (1)
{
cnt++;
err = HAL_SD_ReadBlocks(&hsd, buf, 0, 512, 4);
if(err!=SD_OK)
{
cnt=0;
MX_SDIO_SD_Init();
}
}
}
with it I found a problem on HAL_SD_Init, las line on this function is
SDIO_Init(hsd->Instance, hsd->Init);
return errorstate;
and with this instruction ClockDiv has 0x00 so the SDIO frequency goes to 24MHz and HAL_SD_ReadBlocks have random errors.
I fix it with this:
/* Configure SDIO peripheral interface */
hsd->Init.ClockDiv = 0x76;
SDIO_Init(hsd->Instance, hsd->Init);
return errorstate;
} This way I have 400Khz and HAL_SD_ReadBlocks run ok. I test with 2MHz, 5MHz and 10MHz and everithing is ok, ReadBlocks run right. When I test with 12MHz or more I start to got problems. So, I think the harware is ok (for 10MHz) and I could implement FatFs.
Is there another test to check that HW is Ok?
Regards!
2015-04-21 10:02 AM
Is there another test to check that HW is Ok?
I'd test with working SPL code as a starting point, and I'd probably put pull-ups on the unused pins. Attached is a blind stab at code that should run on the F411, based on code that worked on the STM32F401C-DISCO with a STM32F4-DIS-BB breakout board. Summary: CPU @ 42 MHz SDIO @ 48 MHz (24 MHz external clock), 1-bit, DMA Output via USART2 PA2/PA3 (Nucleo Virtual) @ 115200 8N1 No Card Detect pin support ________________ Attachments : SDIOTEST-NUCLEO-ELGARBE-1BIT-REL1.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I10n&d=%2Fa%2F0X0000000bgr%2FLuO27TvBaG8ZZ1nh.PJdgfnKgekYDedDM3_oQMXo84k&asPdf=false2015-04-21 11:51 AM
Thank clive, have you got source? system workbench project, maybe?
2015-04-21 12:46 PM
Of course I have source, I built it in Keil. It's bound to a bunch of test framework code I'm not sharing. The code is materially similar to that which I've released in Keil and GNU/GCC form for the STM32F4-DISCO series.
I have neither STM32F411E-DISCO or NUCLEO-411RE boards.Does the example work? Should provide read/write timing, and integrity check via a CRC32 of the data that was written vs that read back.2015-04-21 2:54 PM
Clive, I attach a picture of my OSC configuration. Nucleo board have not external XTAL... Is your build compatible with Nucleo osc config?
Thank! ________________ Attachments : Captura_de_pantalla_2015-04-21_18.45.10.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I10i&d=%2Fa%2F0X0000000bgp%2FhYgJJjpygh2SkVP8xZX6p0AKp2wlFo3aa3EiUIVsEHQ&asPdf=false2015-04-21 5:22 PM
But you should be able to get a solid 8 MHz HSE input via the the MCO/PA8 output of the F103 doing the ST-LINK functionality.
Not sure which source I'm using here, or what the default jumpers/bridges on the Nucleo are.