STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Including a pre-compiled image in a project

Posted on October 05, 2015 at 21:35Hi,I am interested in including a sort of fake secure bootloader in my application on the usart, which would purport to offer the option to download the firmware image, but which would actually serve up a fake imag...

estersci2 by Associate III
  • 2482 Views
  • 5 replies
  • 0 kudos

STM32F030x DMA offset by 1 half-word (2 bytes)

Posted on October 09, 2015 at 05:21Hello, I find that DMA works correctly, but that an internal hardware counter (register) [IMHO] starts the DMA off by one word.  Link to example is below.  (i.e. first sample is placed into array[1], last sample is...

walworc by Associate II
  • 1642 Views
  • 2 replies
  • 0 kudos

STM32F103 Update Flash Program from IAP

Posted on October 09, 2015 at 16:32I would like to be able to reprogram the Flash program on my STM32F103 chip via in-application programming. Essentially be able to upgrade the firmware without JTAG or bootloader jumper. I have the PM0075 Programmi...

stm32f429 withsimulink

Posted on October 03, 2015 at 13:26hello every one I'm trying  to program stm32f429 with Simulink and I use matlab 2013a and MAT target 4.2.0 when I have used stm_Config block to configure  hardware target I got a problem that I can’t set the block ...

0690X00000604skQAA.png
abdelaziz by Associate II
  • 1281 Views
  • 3 replies
  • 0 kudos

STM32L0 eeprom writting issue after a page erase

Posted on October 09, 2015 at 13:14Hi, I cannot  write any data into the eeprom after a Erase_page. HAL_FLASH_Program(..) and FLASH_Erase_Page(...) work fine independently. But if HAL_FLASH_Program(...) is called just after FLASH_Erase_Page(), HAL...

tingting by Associate II
  • 1284 Views
  • 4 replies
  • 0 kudos

DMA enabled USART operation on STM32

Posted on October 08, 2015 at 16:23 I'm trying to understand DMA usage by testing a simple application. The idea is to allow USART peripheral to access read and write from and to memory directly, by using DMA technique. I'm testing this on htt...

0690X00000605JCQAY.png 0690X00000605GOQAY.png
gmate1 by Associate II
  • 2754 Views
  • 5 replies
  • 0 kudos

STM32l152c Discovery board, I2C Slave problem

Posted on October 09, 2015 at 13:23 I have I2C slave working to a point but have an event code which causes the isr to trigger continuously. Simplified code below. Now I am using a ''Total Phase Aardvark'' to ask for 8 bytes of data and ...

Comparator on VDD

Posted on October 09, 2015 at 10:47Hi, I'm using a STM32 L051K8 and i'm kind of short in IO, is there any way to avoid using an ADC pin to measure VDD?? #vdd #stm32

poisson by Associate
  • 993 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.