Skip to main content
solsson
Visitor II
April 21, 2015
Question

Receiving CANbus data

  • April 21, 2015
  • 0 replies
  • 360 views
Posted on April 22, 2015 at 01:27

SO I am incredibly confused.  I have an application that uses CANbus.  I have the transmit running fine and I am to the point where I am receiving interrupts when I receive a message.  so I am confused by the lack of documents, but can anyone tell me what the difference is between HAL_CAN_Receive_IT() and HAL_CAN_Receive()?

I have seen code samples with HAL_CAN_Receive in the ISR and I have seen HAL_CAN_Receive_IT in regular code.  I am not sure how to get to the data when I am in the ISR.

I have seen samples that look like this:

CanRxMsgTypeDef RMess;

  RMess.FIFONumber = CAN_FIFO1;

  RMess.FMI = 14;

  RMess.StdId = 0x541;

  RMess.DLC = 0;

  RMess.RTR = 0;

  RMess.IDE = CAN_ID_STD;

  hcan2.pRxMsg = &RMess;

 

  HAL_CAN_Receive_IT(&hcan2,CAN_FIFO1);

  /* USER CODE BEGIN 3 */

  /* Infinite loop */

  while (1)

I don't understand why I would want to pre-populate RMess if I am about to overwrite it with receive data.  I already have a filter.

Can someone please help me understand these APIs and how I get data after the interrupt arrives?

BY the way -- I have a fully operational canbus and several nodes receiving the data and sending me data.  I understand the transceivers and terminations.  I can see the data arriving at the device with the scope and I am getting the interrupt when data arrives.

Thanks

Steve

#c
    This topic has been closed for replies.