cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429-Disco - TP - I2C

feky2
Associate
Posted on April 06, 2015 at 00:26

Hello,

I try to find some topick with same problem. But every topick is without the solution of problem.

I have problem with I2C in 95% (yep, sometimes it works, after restart, it not work). I try to comunicate with STMPE811 via I2C. I setup GPIOs for I2C3 (PA8 and PC3) and I2C3 timing.

// Configure I2C3 (100kHz standard)

I2C3->CCR    =

0xD9

;

// Clock control - Th&Tl = CCR*PCLK => 5us

I2C3->CR2   |= (APB1clk /

1000000

);

// Freq of APB1 in MHz

I2C3->CR1   |= I2C_CR1_ACK;

// Acknowledge returned after

I2C3->OAR1  |=

0x4000

;

// Bit 14 Should always be kept at 1 by software. ?????? WTF!? OK, But why?

I2C3->TRISE  = (APB1clk /

1000000

) +

1

;

// Rise time = 1000ns

// Enable peripheral

I2C3->CR1   |= I2C_CR1_PE;

// Enable peripheral

Next I tryed to read an ID from STMPE811. I set bit START in CR1 and wait for SB bit.

// Generate start condiction

I2C3->CR1 |= I2C_CR1_START;

while(!(I2C3->SR1 & I2C_SR1_SB))

// Wait to SB

Voltages on lines are:

SDA 0.1V

SCL 3.05V

But SB bit is not set, never. It always is stuck in cycle.

Can someone help with it?

Thanks for any response.

#i2c #stm32f429discovery #touchpad
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
fb2
Associate II
Posted on April 21, 2015 at 21:43

Hello, I have the same problem. Did you manage to solve it?

Thank you.

Fernando