STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to detect on-board USB-stick

Posted on October 14, 2015 at 07:09Dear Sir:   How to detect plug in behavior for USB-stick in FW? My project implement a USB MSC host. If USB-stick is on board before power on, the FW can't detect it. I must plug it out and plug in, FW will now det...

Problem with OV7670 (no FIFO)

Posted on October 10, 2015 at 21:52Hi Everyone,I am working on OV7670 module (no FIFO) with STM32F407 chip. Due to I want to get image in 640x480 pixels so I try to manual scan (don't use DMCI). I set REG_CLKRC = CLK_EXT and control clock (set LOW/H...

0690X000006034jQAA.jpg
thanhnt by Associate
  • 1173 Views
  • 1 replies
  • 0 kudos

Error While Flashing Stm32f429

Posted on October 12, 2015 at 14:15Hi!    I have a problem with flashing stm32f429. I using ST LinkV2 on stm32f429 Discovery Board to flash for external stm32f429 board ( that I made) , it have erased successfully, I programmed about 30% and it got ...

0690X00000605JHQAY.png
gds by Associate II
  • 1334 Views
  • 2 replies
  • 0 kudos

STM32CubeF7 bug report

Posted on September 19, 2015 at 23:35Hi,The function SystemInit_ExtMemCtl() in the file system_stm32f7xx.c is not ported to STM32F7-DISCO, since the DISCO and EVAL use different SDRAM, it will not work.Another thing, the SystemClock is configured in...

help: programming the FLASH excess the physical memory size

Posted on October 13, 2015 at 21:12the mcu i used : STM32F105R8T6, the flash size is 64k, according to the PM0075, the last page should be 0x0800 F800 ~ 0x0800 FFFF. However I tried to write and read back the data on page 0x0802 0000 ~ 0x0802 07FFF ...

tcheung by Associate
  • 1187 Views
  • 1 replies
  • 0 kudos

STM32F301K8U6 thermal pad connect to GND?

Posted on October 08, 2015 at 11:07I checked the datasheet and couldn't find the information whether the thermal pad should be connected to board ground, although another engineer told me it is very common to do so. Would anyone please advise whethe...

song by Associate II
  • 1092 Views
  • 2 replies
  • 0 kudos