2015-04-16 6:59 AM
Hi!
I'm using MTF32F030R8 and I need to develope my own bootloader. I use the first 8K of flash for bootloader (from 0x800000 to 0x8001FFF) and from 0x8002000 my SW application. I'm not finding how to set the interrupt vector table at a different address than 0x00000000. Is it possible? How can i do? Thank you Lisa2015-04-16 8:21 AM
You can't relocate the vector table.
What you have to do is copy it to the base of RAM, in a space you've carved out, and map the RAM at ZERO.Look for some IAP examples, or other thread's I've posted to on the forum on this topic.2015-04-16 9:07 AM
I haven't tried this, but -
There is a register called VTOR, the vector table offset register, that holds a 30 bit offset that is used to calculate the address of the vector table. VTOR points at a 128 ''word'' aligned table, you will have to figure out what a word is in this architecture.This sort of thing is essential when working with bootloaders and RTOS'.The 68000 family had a register called VBR, the vector base register, that did the same thing.2015-04-16 6:07 PM
There is a register called VTOR....
And the Cortex-M0 doesn't have this.2015-04-16 6:11 PM
Thread that's on point, there are others too, use Google the search here sucks.
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F051K6%20NVIC_SetVectorTable&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=59]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FSTM32F051K6%20NVIC_SetVectorTable&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=59We’re moving the ST Community to a new platform to give you a better and more reliable community experience.