STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Watchdog reset while changing CLock frequency

Posted on October 14, 2015 at 16:13I have configured my stm32f427 microcontroller,  Sysclk to run in a clock frequency of 60mhz(HSI and PLL). I have reduced it to 16mhz (Sysclk directly from HSI). While executing this code watchdog resets. Below men...

jijo137 by Associate II
  • 1323 Views
  • 2 replies
  • 0 kudos

SPI readout of a sensor

Posted on October 12, 2015 at 01:55Hi, I am trying a very simple thing: I would like to read a register of a sensor. So the first thing I did is to write the read-register (8 bit) to the sensor. After that the DR register has been filled with dummy...

USART RX interrupt driven ring buffer

Posted on October 14, 2015 at 08:51Hey guys. First of all im new to this kind of stuff, so dont judge me please. I've been working for days on USART. I learned to transmit and receive strings via usart in normal mode, but as i try to do it with inte...

e239955 by Associate II
  • 3601 Views
  • 5 replies
  • 0 kudos

Multiple ADC STM32F303 discovery board

Posted on July 09, 2013 at 23:45The original post was too long to process during our migration. Please click on the attachment to read the original post.

marko by Associate II
  • 4881 Views
  • 10 replies
  • 0 kudos

I2C on stm32f301

Posted on October 06, 2015 at 11:50I've started development of an application on an STM32F3 discovery baord, and am moving onto the target board, which uses an STM32F301. I can't get the I2C peripherals to run. If can bit-bash I2C on the GPIO, but ...

artgodwin by Associate II
  • 1156 Views
  • 2 replies
  • 0 kudos

bootloader with read protection

Posted on October 14, 2015 at 14:40I wrote a bootloader (STM32F4), that takes a file from USB memory, and updates the system firmware.I would like to have read protection. However when protection option is on(level 1) when writing the new firmware t...

Johanan1 by Associate II
  • 835 Views
  • 0 replies
  • 0 kudos

Sampling Time

Posted on September 20, 2015 at 12:50Hello everyone !I've successfully connected stm32f4 discovery board with Matlab R2015a Simulink, but when i make a block diagram for generating simple pwm on simulink and set the sampling time of 0.1 milli second...

STEMWIN SHOW IMAGE FROM SD CARD

Posted on October 09, 2015 at 14:36Hello! I am working in a project that uses a STM32F407 and 7'' TFT LCD with SSD1963 controller, after hard work to put the LCD running and some corrections on the board, now we are trying to display a image from a ...

giovani by Associate II
  • 2021 Views
  • 3 replies
  • 0 kudos