Question
STM32F072CBT6 Reset
Posted on April 17, 2015 at 10:48
Hi there
I designed a print with a STM32F072CBT6 and connect with a Discovery Board.First I designed the software on the Discovery Board. After that, i want to test the connection to the CBT6. My Code works fine on the first try but after disconnect, the mcu starts itself after 5ms, repeating itself and i cant connect with to stop an reprogram it. Is there a way to force the chip to reset/flash the rom?My IDE is the free version of KeilMy Startup Code:/* Includes ------------------------------------------------------------------*/&sharpinclude ''stm32f0xx_hal.h''/* USER CODE BEGIN Includes *//* USER CODE END Includes *//* Private variables ---------------------------------------------------------*/UART_HandleTypeDef huart1;DMA_HandleTypeDef hdma_usart1_rx;DMA_HandleTypeDef hdma_usart1_tx;/* USER CODE BEGIN PV *//* USER CODE END PV *//* Private function prototypes -----------------------------------------------*/void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_DMA_Init(void);static void MX_USART1_UART_Init(void);/* USER CODE BEGIN PFP *//* USER CODE END PFP *//* USER CODE BEGIN 0 *//* USER CODE END 0 */int main(void){ /* USER CODE BEGIN 1 */ uint8_t aTransmitBuffer[3]; aTransmitBuffer[0]=0x55; aTransmitBuffer[1]=0xFF; aTransmitBuffer[2]=0x32; /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_USART1_UART_Init(); /* USER CODE BEGIN 2 */ HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET); HAL_UART_Transmit_DMA(&huart1, &aTransmitBuffer[0], 3); /* USER CODE END 2 */ /* USER CODE BEGIN 3 */ /* Infinite loop */ while (1) { } /* USER CODE END 3 */} #external-reset