STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NucleoF411re, SPI1 --> NSS (StdPeriphLib)

Posted on October 30, 2015 at 17:33Hello guysim working on a SPI interface where SPI1 has a hard wired NSS (neg. slave select == /chip select).watching the logic analyser, the spi transmission takes place but the NSS signal is staying high during th...

60 mA at +/- 1.5V on GPIO on a NUCLEO-L053R8

Posted on October 30, 2015 at 20:03Dear all,I am a beginner and my questions may seem stupid, so please understand.Using mbed, I would like to program a NUCLEO-L053R8 evaluation board. The goal is to deliver 60mA@1.5V on a group of GPIO and change i...

Valid Stack Pointer Regions for STM32 MCU

Posted on October 30, 2015 at 19:01Hello, since a week, I always get a HardFault in the line ''bx R14'' of the FreeRTOS 8.2.2 assembler routine vPortSVCHandler on a STM32F103zg. ''Attempt to do exception with bad value in EXEC_RETURN number (INVPC)...

Nucleo 64 PCB information

Posted on October 30, 2015 at 15:37Folks Does anyone know of where there is  PCB data for a Nucleo 64 daughter board I do not use Altrium designer so looking for a different format as data given by ST is a binary output file rather than an easily tr...

dcurran2 by Associate II
  • 1178 Views
  • 1 replies
  • 0 kudos

DAC unfiltered output

Posted on October 30, 2015 at 16:12Hi every 1.I am trying to implement the sine wave generator on STM32F3 which is actually working fine but the problem is that theoutput waveform is not identical to the real time function generator because its not ...

0690X0000060353QAA.jpg
ameer by Associate II
  • 1995 Views
  • 3 replies
  • 0 kudos

PWM: Help on PWM setup to prevent off duty cycle

Posted on October 28, 2015 at 15:57Hi allWe need some help on a PWM setup. I�ll first present the use case then the issue we�re having and code. I�m pretty sure this is a PWM/timer understanding/register setup issue, but I just can figure out what i...

0690X00000605JgQAI.png
kimtommy by Associate II
  • 1915 Views
  • 2 replies
  • 0 kudos

Problem with PWM

Posted on October 30, 2015 at 08:37 Hey there. For few days i've been trying to successfully init PWM, but i didnt managed to do it. It looks like i saw all of the examples on the internet. I want to init simple PWM channel with timer on L...

e239955 by Associate II
  • 911 Views
  • 1 replies
  • 0 kudos

BlueMS source code

Posted on October 30, 2015 at 10:46Hi,I am working with bluemicrosystem1 application,for further expansion of my project BlueMS app source code is mandatory.In some of the sites it showing as it is available on Github. Anyone have this source code?P...