STM32F4 - SPI unidirectional receive only
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-06-16 5:25 AM
Posted on June 16, 2015 at 14:25The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-06-16 7:59 AM
Posted on June 16, 2015 at 16:59
Okay, some small progress:
The OVR bit most likely comes from the debugging process where the SPI kept receiving data while the CPU was halted at a breakpoint. I'm starting my transmissions from a timer overflow interrupt. I now disabled the timers during halt at breakpoints by executing DBGMCU_APB1PeriphConfig(DBGMCU_TIM2_STOP, ENABLE); in the init code. Now I can successfully restart the transmission. I set the SPI prescaler to 32, and now the CPU is able to actually catch the interrupts. So most of my problems are fixed. Only one remaining is that I still only receive 0x00 even though I can definitely say that there is data arriving at the pin.