STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DAC unfiltered output

Posted on October 30, 2015 at 16:12Hi every 1.I am trying to implement the sine wave generator on STM32F3 which is actually working fine but the problem is that theoutput waveform is not identical to the real time function generator because its not ...

0690X0000060353QAA.jpg
ameer by Associate II
  • 2023 Views
  • 3 replies
  • 0 kudos

PWM: Help on PWM setup to prevent off duty cycle

Posted on October 28, 2015 at 15:57Hi allWe need some help on a PWM setup. I�ll first present the use case then the issue we�re having and code. I�m pretty sure this is a PWM/timer understanding/register setup issue, but I just can figure out what i...

0690X00000605JgQAI.png
kimtommy by Associate II
  • 1931 Views
  • 2 replies
  • 0 kudos

Problem with PWM

Posted on October 30, 2015 at 08:37 Hey there. For few days i've been trying to successfully init PWM, but i didnt managed to do it. It looks like i saw all of the examples on the internet. I want to init simple PWM channel with timer on L...

e239955 by Associate II
  • 927 Views
  • 1 replies
  • 0 kudos

BlueMS source code

Posted on October 30, 2015 at 10:46Hi,I am working with bluemicrosystem1 application,for further expansion of my project BlueMS app source code is mandatory.In some of the sites it showing as it is available on Github. Anyone have this source code?P...

where is the 2nd I2C interface of STM32F103?

Posted on October 29, 2015 at 08:59Hi all,Recently I am working on a demon code using STM32F103.In this demon code,it defines the PE2, PE3 as the I2C interface, as below:/* Configure I2C pins: PE2->SCL and PE3->SDA */ GPIO_InitStructure.GPIO_Pin = G...

laojian by Associate II
  • 1989 Views
  • 2 replies
  • 0 kudos

Writing SD card raw level

Posted on October 30, 2015 at 06:50Is that possible to Write an SDCard at raw level without using FAT File system? if yes, how? is there any sample code? i am using stm32f4 #sdcard-stm32f4-sdio-fatfs

problem with pulse width measurement

Posted on October 29, 2015 at 23:06Hi, It seems there is a problem when I try the example project regarding using TIM input capture mode to measure pulse width. In example project, the both edge triggering mode is used. My question is how to set it ...