STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can the interrupt vector table be saved and/or reloaded?

Posted on November 08, 2015 at 22:53Hi, I am running a function that seems to be moving the default vector table, that has been set up for FreeRTOS. After running  these 2 functions, USB_MSC_HOST_Init(), and then MSCHOST_DeInit(), I run SystemInit()...

open an AC6 project

Posted on November 09, 2015 at 16:23Hello, In a Cube project folder, when I click *.uvprojx, the project opens in Keil toolchain ; I build (0 error, 0 warning, great!!), and ready to run. Likewise when I click *.eww and IAR toolchain.What do I click...

STM32F302R8T6 minimal circuit Help

Posted on November 02, 2015 at 04:06Hi, I am very new to ST microcontrollers and wanted to know if someone can help me with a schematic for the STM32F302R8T6. The hardware I am designing is a USB to CANBUS tool but I need to know whats the minimal c...

HAL_UART_Transmit_IT not working as expected

Posted on November 09, 2015 at 11:00 Hello I try to debug my application using printf I write some code to overwrite fputc. My problem is with the function HAL_UART_Transmit_IT of the HAL module It doesn't succeed to s...

UM1472 (STM32F4 Discovery manual) Correction

Posted on November 09, 2015 at 02:03Regarding http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00039084.pdf - the user manual for the Discovery kit for STM32F407/417 lines: On page 20, in section 4.11 ''Solder b...

STM32F746G-DISCO LibJpeg

Posted on November 09, 2015 at 13:00I use LibJpeg on board F7. I have a few questions. In reference example used an image 240x320, but my display is 480x272. I changed http://vk.com/feed?section=search&q=%23define for new picture and increased line...

Bootloader USB settings

Posted on April 13, 2015 at 12:11The original post was too long to process during our migration. Please click on the attachment to read the original post.

mathilde by Associate
  • 2526 Views
  • 3 replies
  • 0 kudos

STM32F7 discovery SD card access

Posted on November 07, 2015 at 14:59Hello, I try to access to the SD card with BSP drivers. BSP_SD_Init and BSP_SD_ReadBlocks return SD_OK, but the read buffer does not reflect the values in SD (the buffer is almost always 0). Can you help me ? Than...