STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hex file for production

Posted on January 23, 2014 at 15:47I am using the STM32L100. How I can combine the hex file for my bootloader with the hex file for my application into one hex file for production? #spi-program

lee by Associate II
  • 5552 Views
  • 12 replies
  • 0 kudos

Serialize eui-64 programming method

Posted on November 10, 2015 at 18:30Hello guys,I'm designing a STM32L-based board and I'll need to implement a different EUI-64 address into the EEPROM and write protect it during production.Could someone tell me what would be the best approach to a...

stm32f4 USART

Posted on November 10, 2015 at 18:32 Hello Every one! Can any 1 please help me with USART data transfer.. The problem is i want to transfer 16 bit value which is saved in global variable to computer from USART. i am trying this void usa...

puneethj by Associate II
  • 2616 Views
  • 2 replies
  • 0 kudos

Power Voltage Detector(PVD) and PA0-WKUP PIn of STM32F100

Posted on November 10, 2015 at 14:54Good morning,  Someone have try to enable the PVD function, and use the PA0-WKUP  Pin like an Output ??  When i start the PVD functions  although i disable the Wake Up pin  (PWR_WakeUpPinCmd (DISABLE);) I am not a...

B.Michele by Associate III
  • 884 Views
  • 0 replies
  • 0 kudos

fsmc pins

Posted on November 10, 2015 at 11:38LCDs use my 8 bit data bus. rs rw cs rd and which pins are the 8-bit data bus? Thank youhttp://i.hizliresim.com/RBv157.png

kemal by Associate II
  • 1299 Views
  • 2 replies
  • 0 kudos

STM32F439I-EVAL no power on USB

Posted on November 09, 2015 at 23:54Running the demonstration project from STM32Cube and tried to load pictures from USB disk. Power does not turn on for USB HS port. Traced the problem to CPEN pin on USB3300. Anybody have a similar board, and does ...

lasse by Associate II
  • 1032 Views
  • 1 replies
  • 0 kudos

Does USB OTG Require Pullup on DP line?

Posted on November 02, 2015 at 05:02 Does the Discovery board use pull-up or pull-down resistors on the USB OTG? Schematic says it doesn't, the USB standard says it's required. Any guesses? Thanks...

stm32 spi

Posted on November 10, 2015 at 11:26Hi.I am tying to connect my STM32F4 (or F1) with external ADC. Data from ADC can be received by SPI after ADC set ''ready'' flag.So the task for controller is to read by SPI 16 bit data on external event.The easie...