STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cube Firmware Error in osPoolAlloc function in cmsis_os.c

Posted on July 14, 2015 at 00:42In the latest version of the STM32CubeF4 package (and the last few I've used), there seems to be an error in the CMSIS OS wrapper for FreeRTOS. I imagine this is in the other Cube packages as well, though I haven't lo...

CAN FILTERS

Posted on November 11, 2015 at 17:48 Hi every one, especially Mr.Clive, today i have problem with CAN FILTERS i want to allow all IDS from 100 to 1FF in other words block all messages after 0x0200 here is my code, Please help me, Thanks in ad...

puneethj by Associate II
  • 1394 Views
  • 1 replies
  • 0 kudos

Connect two timers in Gated Mode

Posted on November 10, 2015 at 09:42Hi, unfortunately I haven't understood how to connect two timers. I want to achieve a 3,2kHz PWM switch signal that turns on and off a 1 MHz signal. I try to setup TIM3 as a master timer; in STM32CubeMX I have sel...

smrtkai by Senior
  • 2206 Views
  • 4 replies
  • 0 kudos

stm32f4 Timer

Posted on November 10, 2015 at 17:34Hello every one! How can i check if the timer is already running.. which flag to use I am trying thisif (TIM2 -> CR1 == TIM_CR1_CEN){// turn led on blue} else{// turn led red on}but it does not work, please help m...

puneethj by Associate II
  • 1864 Views
  • 6 replies
  • 0 kudos

modbus tcp port lwIP stack on stm32f4 with DP83848 PHY

Posted on November 05, 2015 at 16:32Good afternoon everyone,I am fairly new to this forum.So hi everyone :) I am a young electronics and embedded systems engineer, used to driver dev but really a noob when it comes to internet networks understanding...

Bootloader - jump to APPLICATION_ADDRESS

Posted on October 30, 2015 at 14:22 Hi, I'm having some issue loading my application from the APPLICATION_ADDRESS -Using a STM32F4 Discovery board -As bootloader application I'm using the STM32F4 example http://www.st.com/...

paul2 by Senior
  • 5820 Views
  • 11 replies
  • 0 kudos