STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4, OPAMP calibration

Posted on November 07, 2015 at 16:53 Hello Has anyone gotten the OPAMP calibration with STM32L4 (or similar) controllers working so far? I've initialized OPAMP1 as PGA with just a positive input and simply called the HAL function for cal...

STemWin keyboard message

Posted on November 17, 2015 at 10:26I create a new child dialogue with function GUI_CreateDialogBox. How to prevent the messages from the keyboard to the parent dialog not arrive. I need to handle message only in a child dialogue. Thank you for your...

jiri by Associate II
  • 791 Views
  • 0 replies
  • 0 kudos

Data transfer from GPIO port to RAM buffer using DMA upon receiving a trigger signal on the timer capture input channel.

Posted on August 07, 2013 at 06:47 Our requirement is to configure the DMA so that it transfers data from the GPIO lines (8 bit data lines) to the RAM buffer upon receiving a trigger signal on the timer capture input channel.We had received an exa...

vimal by Associate
  • 12792 Views
  • 19 replies
  • 0 kudos

Question regarding PWM

Posted on November 14, 2015 at 19:02Hi.I'm using timer in PWM mode to control LED. If output is always 1 (CCR register is equal to ARR), LED is green. If output is 0 (CCR is always 0), LED is red. If I set duty cycle to 50% at high frequency, LED is...

matic by Associate III
  • 2392 Views
  • 8 replies
  • 0 kudos

SMBus Alert

Posted on November 16, 2015 at 16:39 Hi guys, some days ago I had a similar question[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/I2CSMBus%20doesn%27t...

0690X00000605JhQAI.png
arapp1990 by Associate II
  • 1637 Views
  • 0 replies
  • 0 kudos

Watchdog with low power mode

Posted on November 16, 2015 at 15:08Hi everyone,I am using the STM32L152 MCU. I am trying to implement a watchdog on my low power module (in stop mode).The device only wakes up on interrupt in order to optimize power consumption.I saw differents top...

alexis by Associate
  • 1040 Views
  • 0 replies
  • 0 kudos

STM32L_Discovery Multichannel ADC example

Posted on November 09, 2015 at 12:38I have been trying extend Clive1 ADC_DMA example on STM32L_Discovery to do multi-channel conversion. But am struggling to get the NVIC_IRQ Handle for the two channel right. Can someone assist me with an example of...

idris by Associate II
  • 2887 Views
  • 6 replies
  • 0 kudos

STM32Cube bug generation new project for MDK V5

Posted on October 30, 2015 at 10:17Hi, When generating a new MDK V5 project with Cube V4.11, the ''Name of Executable'' in ''options for target/output'' will left empty but t his is a mandatory field and need a value. Normally is this value ''[Proje...

Osto by Senior
  • 1087 Views
  • 2 replies
  • 0 kudos