STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Missing BlueNRG driver for NUCLEO-F103RB?

Posted on November 17, 2015 at 11:18Dear all,I have a NUCLEO-F103RB together with a X-NUCLEO-IDB04A1 Bluetooth extension board.Now I wanted to start learning how to program with bluetooth and downloaded x-cube-ble1.zip from STM website.Inside the fo...

timon by Associate
  • 843 Views
  • 1 replies
  • 0 kudos

STM32F030R8 TIM3 remap to port C

Posted on November 17, 2015 at 09:58Hi guys I referred to the timer 3 channels remapped to port C for STM32F030R8. The datasheet DM00088500 version 2 page 30 did not mention there is a restriction for the mapping, while page 37 do carry a small (1) ...

V CORE domain clocks

Posted on November 17, 2015 at 18:55In document DM00108282.pdf(RM0377) page 143 it mentions V CORE domain clocks. What clocks are included in V Core domain? What clocks are included in Vdd domain?

bigbird by Associate
  • 1172 Views
  • 1 replies
  • 0 kudos

stm32f401re nucleo: USART programming

Posted on November 16, 2015 at 11:38Hello everybody,I'm new on the forum and on ST microcontrollers.I'm trying to program the USART in assembly, but I have some issue to write on DR.What am I missing? Somebody can help me, please?*******************...

life758 by Associate II
  • 1930 Views
  • 6 replies
  • 0 kudos

STM32 stop mode and UART interrupt

Posted on November 18, 2015 at 08:18Hi 1. Can a UART receive interrupt wake the STM32 MCU from Stop mode (RX line start bit) ? 2. Only a External Interrupt can wake the STM32 MCU from low power modes ? Regards #!stm32f4-disco #low-power-stop-mode

RTC Wakeup interrupt not triggering on STM32L100

Posted on November 17, 2015 at 15:09Hello,It seems that the IRQ handler for the wakeup does not trigger even the RTC is running correctly, WUTIE is set in CR register and the ISR flag WUTF is set as expected. What could be the issue? The FW is build...

juho by Associate II
  • 1719 Views
  • 2 replies
  • 0 kudos

STM32F4-Discovery Boot0/1 De-soldering

Posted on November 17, 2015 at 23:37Greetings,I'm wanting to shave every bit of power I can off of this board and was thinking of de-soldering the Boot0 and Boot1 bridges.  Question is, will this adversely effect the bootloader in any way?  Currentl...

shawn2 by Associate II
  • 708 Views
  • 0 replies
  • 0 kudos

STM32F4 Timer External Pulse counting

Posted on May 18, 2013 at 00:23Since 4 day I'm trying write code which will be able to count external pulses. I tried to use encoder mode but i supposed that this work only with 2 quadrature encoders. I have only one pulse signal and i have no idea ...

STM32f4 discovery board

Posted on November 16, 2015 at 17:27Hello,I have a problem with running a  TFT. My LCD chip is SSD1289 . I have communication between the board ( stm32f407 - discovery ) and the LCD but there isn't a text on the screen. I attach my code.