cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 ADC Triple Mode with DMA

pant
Associate II
Posted on June 24, 2015 at 16:11

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
raptorhal2
Lead
Posted on June 24, 2015 at 16:52

It helps to read the fine print in the Reference Manual, especially when the author anticipated your reaction with a typo.

''DAM mode 2 is used in interleaved mode and in regular simultaneous mode (for

Dual ADC mode only).''

Cheers, Hal

pant
Associate II
Posted on June 24, 2015 at 19:13

Dear Hal,

Thank you very much for your answer, but I didn't really get it. I had seen that part and I thought of it as if I can use DMA mode 2 in Triple ADC mode however I want, but in Dual ADC mode only in interleaved and regular simultaneous mode. And actually exactly above the part you mentioned with the nice typo :) it says how the DMA requests are generated in Triple mode.

Excuse me if I mixed it up.

Regards,

Pantelis