Posted on June 15, 2015 at 14:09
i want to build Audio_playback_and_record project for usb library but there are some problems. i downloaded this project (stsw-stm32zip) from
http://www.st.com/web/en/catalog/tools/PF257904#.
i have changed...
Posted on December 19, 2014 at 10:04
hi, i want to set an offset value to vector table of my application for writing a custom bootloader.
i set it with VECT_TAB_OFFSET definition in thesystem_stm32f4xx.c file like following:
#define VE...
Posted on November 29, 2014 at 12:54
i have custom board with STM32F427VI and want to boot from usart3 via bootloader inside system memory.
boot0 pin is low and boot1 pin is NC. i dont want to switch boot pins. because eventually these pi...
Posted on August 28, 2015 at 14:06when i implement this (VCP) project, can i use my microcontroller both in device and host modes? because OTG feature of USB peripheral tells us that we can use in both modes if i dont misunderstand.
Posted on June 25, 2015 at 13:22i have checked options and paths. re add the files back but none of them work. but i have found the solution by chance.right click the folder/file that signed with cross then click on options. then uncheck ''exclude f...