STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32 DMA request per channel + multple peripherals

Posted on November 23, 2015 at 16:16 Hi, I would like to use the DMA with diferent peripherals of a stmHere are the resuming points. target MCU: STM32L0 purpose : Dma + uart1+uart2+uart3 +spi+i2c For instance i succeded con...

r2s by Associate II
  • 1980 Views
  • 3 replies
  • 0 kudos

HAL_SPI_transmit 32 bytes ?

Posted on November 22, 2015 at 22:33  The original post was too long to process during our migration. Please click on the attachment to read the original post.

Output Compare + Cube + HAL

Posted on November 23, 2015 at 16:00Hi to everyone. I'm struggling with OC mode on STM32F4 Discovery, in order to get high level on one of the pins with specified delay, so i chose OCM ''active level on match''. At first start everything is fine, bu...

STm32L151 temperature sensor example

Posted on November 23, 2015 at 14:57I am new to STm32 architecture. Trying  to get the internal temperature sensor going. I am using a STm32L151VC microcontroller, STM32-QFP100 programmer adapter and IAR tool chain. I am trying to use the following ...

tanim330 by Associate
  • 853 Views
  • 0 replies
  • 0 kudos

STM32F0 IAP function

Posted on November 19, 2015 at 12:31Hi all I try to implement a boot loader that can be jump to user application of STM32F030R8 chip , and I find the IAP sample as follow.http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF2581...

jeff0118 by Associate II
  • 1830 Views
  • 3 replies
  • 0 kudos

STM32F439xx Dual Bank jump

Posted on November 12, 2015 at 13:54Hello,I have 2 custom application codes, one for bootloading and the other for the functional app. Bootloader resides in the first flash mem sector 0x8000000.If the app resides inside the first mem bank (same as b...

afduarte by Associate II
  • 1012 Views
  • 1 replies
  • 0 kudos

STM32-MAT/TARGET Compiling using simulink error

Posted on November 20, 2015 at 20:40 Hi, I am trying to use simulink to generate code for my STM32F4DISCO. I have the STM32F4Discovery addon on matlab. I have the STM32-MAT/TARGET with the patch. STM32CubeMX and Atollic studio are insta...

marcelo by Associate
  • 1093 Views
  • 1 replies
  • 0 kudos

No page erase in STM32F215

Posted on November 23, 2015 at 09:33Hi Guys,I am not able to find any option for page erase of internal flash in docs as well as examples. Is it that the STM32F215 MCU supports only sector and chip erase for its internal  flash.regards,Sanjeev

chota by Associate
  • 878 Views
  • 2 replies
  • 0 kudos

USB HS HOST Error

Posted on November 21, 2015 at 18:40The original post was too long to process during our migration. Please click on the attachment to read the original post.

geladari by Associate
  • 939 Views
  • 2 replies
  • 0 kudos