cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK/V2 firmware upgrade

rbcs
Associate II
Posted on July 06, 2015 at 18:03

Hi, I am new to working with the ST LINK.

I downloaded the ST-LINK/V2 firmware upgrade from the site. When attempting to run the jar file I got an error:

    ''Architecture not supported(arm)''

Could someone please help
This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on July 06, 2015 at 20:16

Assume we know nothing about your system, or the specific file you downloaded.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
rbcs
Associate II
Posted on July 08, 2015 at 13:33

I am running the raspberry pi b+ v1.2

The file I downloaded was:

Part Number - STSW-LINK005, Version - 2.24.4,

Posted on July 08, 2015 at 14:49

The error suggests it's expecting an x86 based system.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
rbcs
Associate II
Posted on July 08, 2015 at 16:41

Yes, I thought as much.

I have trace the problem to a driver(libSTLinkUSBDriver.so) that was compiled for x86 and x64. Is there however any way to get it to work with arm

Posted on July 08, 2015 at 19:43

Is there however any way to get it to work with arm

I doubt there's a strong commercial driver, your use case is a bit of an outlier. Perhaps they are using GPL code requiring the release of source?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..