cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX STM32CubeF0 update

yuvalk
Associate II
Posted on July 07, 2015 at 15:24

Hi,

I've just updated CudeMX to v4.8 and noticed that the latest version of STM32CubeF0 firmware package is 1.2.1, while in ST website there version 1.3.0 is available.

I tried to install it manually with no successes.

Any solution?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on July 07, 2015 at 15:34

Does the internal mechanism to download new libraries function?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
yuvalk
Associate II
Posted on July 08, 2015 at 07:46

Yes, it does. It updated the CubeMX version and the F4 library.

yuvalk
Associate II
Posted on July 08, 2015 at 07:48

BTW, if you look on the CubeMX web page, you'll notice the release notes are for version 0.49 while the download is 4.8.

When I tried to install the F0 library manually, I got a message saying I cannot do it on this CubeMX version. 

chrif
Associate II
Posted on July 08, 2015 at 14:46

Hi,

As indicated in the official response of ST team, the CubeMx has a limitation. it supports only one firmware version. Havec alook to this discussion[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Hou%20to%20use%20old%20package%20version%20on%20STM32CUBEMX&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&currentviews=46]Discussion

Regards