STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f405xx CAN Remote frame

Posted on November 25, 2015 at 05:32Hi ,I'm usingaSTM32F405,my purpose is to receive the remote frame .but FIFO0 is not to receive the message . Namely , the function ''CAN2_RX0_IRQHandler'' interrupter is not access. My CONFIG is:  hcan2.Init.Mode ...

STM32F373 SDADC2,3 problem

Posted on October 06, 2014 at 07:48  The original post was too long to process during our migration. Please click on the attachment to read the original post.

sum by Associate
  • 871 Views
  • 1 replies
  • 0 kudos

STM32F4-Discovery: R30 (Boot0) Value. What is acceptable?

Posted on November 19, 2015 at 20:09I'm developing a low power solution using only the devboard, however I'd like to be able to buy some mA by increasing the value of R30.  Would changing this to say a 10k SMT effect anything?  Alternatively, the on...

shawn2 by Associate II
  • 1505 Views
  • 3 replies
  • 0 kudos

STM32F4 CAN filtering

Posted on November 24, 2015 at 18:06Hi, I'm using a STM32F407, I'm implementing the CAN communication. My purpose is to receive only one type of message and filter out all other messages. I can not understand which settings to use for filtering mess...

vlr by Associate II
  • 979 Views
  • 1 replies
  • 0 kudos

Std periph library for f7

Posted on November 24, 2015 at 18:42 Hi, I'm porting SPL and ETH to stm32f7 for use in my project, but I've no idea about USB. I put library source code on gitlab, you can get it here https://gitlab.com/caesar-lab/stm32f7-legacy-library...

dechawat by Associate II
  • 716 Views
  • 0 replies
  • 0 kudos

STM32L4 CMSIS Std Periph Library Available?

Posted on November 23, 2015 at 22:28Hi, Can someone please advise on the availability of the std peripheral libraries for the STM32L4 device? That is, HAL-free?  I couldn't find any in the package that i got from the ST website that claims there is ...

RS485 modbus Communication with Nucleo

Posted on November 24, 2015 at 17:05Hello Everyone.I would use the NUCLEO l152re board to implement the Modbus via RS485 and communicate with one or more slaves.Right now I would need of MODBUS master library for STM32 NUCLEO.Is there anyone that ca...

DMX-512 RECEIVER

Posted on November 24, 2015 at 17:03HiI'm trying to receive dmx512 with a stm32f100rb (discovery board). I can't detect the break. Please help me :'(I try to detect the break with timers but my results are bad.... If someone can explain me how to de...

Problem loading code

Posted on November 24, 2015 at 09:51Hello,I' m programming stm32f103RB and my code goes well but I'm doing some changes and when I try to load the code the IAR show my this error:* Programming failed @address 0x0800400 (program error)I don't know wh...

msanchez by Associate II
  • 971 Views
  • 1 replies
  • 0 kudos