STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

No way to set SysTick to -1 priority in STM32CubeMX

Posted on December 24, 2015 at 08:02I'm using STM32CubeMX (V4.12.0) and targeting an STM32F411. By default, SysTick has an IRQ number of -1 which makes it higher priority than an interrupt with Preemption priority of 0, SubPriority of 0. I would li...

STM32F103C8T6 SPI DMA hardfault

Posted on December 24, 2015 at 08:31Hello All,I try to send an uint8_t array over SPI with DMA, but the microcontroller going to hard fault handler. The C code is generated by STM32cubeMX.My source code is:/* USER CODE BEGIN 0 */&sharpdefine meret 1...

to create stable signal problem with stm32F415RG

Posted on December 16, 2015 at 14:49 I'm doing a project that is based on the creation of signals with great precision frequency from a 32-bit microcontroller ARM Cortex M4 manufacturer ST, the (STM32F415RG) family. What I'm looking for is accura...

fjs71 by Associate II
  • 3105 Views
  • 10 replies
  • 0 kudos

stm32f7discovery cubemx driver ethernet LAN8742a

Posted on December 22, 2015 at 13:04Hello All,When I generate code with  stm32cube for kit stm32f7discovery in filestm32f7xx_hal_conf.h is generated driver for  DP83848_PHY_ADDRESS 0x01 , not for lan9742acan you help me ?Thank you

vrba1 by Associate
  • 808 Views
  • 1 replies
  • 0 kudos