STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Going into hard fault handler when missing interrupt

Posted on December 24, 2015 at 10:49Hello I have configured the board for the rising edge interrupt but the slave does not support it. It requires host GPIO to be configured in active high level trigger mode. Because of this some times I am missing...

keyur by Associate
  • 1694 Views
  • 2 replies
  • 0 kudos

SPI on STM32F4 Discovery and STM32F429

Posted on September 10, 2015 at 12:45Please help me for this situation.I am using both STM32F4 DISCOVERY and CORE STM32F429 board fromhttp://waveshare.com/I use SPI standard driver to read ADS1292 chip from TI but I have a tricky problem.SPI2 was us...

linhnd89 by Associate II
  • 3711 Views
  • 9 replies
  • 0 kudos

F103 USART1 RX IRQ happens premature.

Posted on December 26, 2015 at 01:55I am using the USART1 interface of an F103 and I'm havin trouble getting interrupts correctly. When receiving a byte the first interrupts get triggered while bit 6 is still underway and then a second interrupt hap...

zhausq by Associate III
  • 1278 Views
  • 3 replies
  • 0 kudos

Configure ADC with HAL for 44.1kHz

Posted on December 27, 2015 at 04:52I want to configure the ADC on my stm324f49i-discovery board to sample audio signal using HAL drivers.  I need a 44.1kz (or 48khz) sampling frequency, but am not sure how to set that up.  My board is running at ma...

spi problem

Posted on July 06, 2015 at 14:37i am using stm32f030c8t6 device .i communicate with external memory ic on spi bus.i am using stmcube32 and mdk-5.for testing purpose i read its id using spi.i am using spi2. at first am not able to generate clock for ...

karan by Associate III
  • 2464 Views
  • 5 replies
  • 0 kudos

windows gets hanged in USB MSC (with uSD) example

Posted on December 25, 2015 at 23:45Hello, For USB Mass storage, I've followed [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/USB%20CDC%20on%20STM32L%20device%20%...

Systick delay weird behavior. [STM32F103CB] [GNUArmEclipse]

Posted on December 26, 2015 at 00:51I am experiencing weird behavior from my systick delay function.The following code does not work.void delay_ms(int time_ms){ uint32_t time_done = SystemUptime+time_ms; while(SystemUptime < time_done) { }}However t...

zhausq by Associate III
  • 848 Views
  • 3 replies
  • 0 kudos

Driving LCD panel with stm32f7

Posted on December 26, 2015 at 17:18Hello, I am designing a board  with a STM32F7 to interface a LCD 800x600, LVDS input. So I use a sn75LVDS84. But I want to know how wire RGB port and LVDS converter. At now I use RGB666 format (R[7..2], G[7..2], B...

aurelien2 by Associate II
  • 1284 Views
  • 0 replies
  • 2 kudos

Interfacing STM32F103ZE to SD Card

Posted on December 23, 2015 at 18:06The original post was too long to process during our migration. Please click on the attachment to read the original post.

mohamed2 by Associate II
  • 3060 Views
  • 5 replies
  • 0 kudos