STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F207ZG and STM32F407ZG compatibility

Hello everyone,I am currently using the STM32F207ZG in my project, but I am considering replacing it with STM32F407ZG due to speed.After reviewing the two MCUs, I found that the cores and memories of the two MCUs are different, but the peripherals ar...

rndkd1 by Associate II
  • 2016 Views
  • 4 replies
  • 6 kudos

Resolved! How to set the clock source for TIM3

How to set the clock source for TIM3 We are trying to use TIM3. We also want to use an external CLK as the clock source for TIM3, but we don't know how to set it. .ioc file - Where should I change the TIM3 clock source settings?

stm32g474met3 keeps burning out for unknown reason

i have MCU circuit with stm32g474met3 as the processor, designed such that it controls the main board charging circuit and it keeps burning randomly at random times could be 5 hours or 20 minuts or even few days I cant figure out why, it burns whethe...

Untitled design (1).png
Tom12 by Associate II
  • 2351 Views
  • 7 replies
  • 0 kudos

STM32l476 boot inquiry

Hello,The STM32L476 MCU is not booting, and it seems to be stuck at address 0x08000228, as shown in the attached image. It used to boot and work correctly before.At some point, it stopped booting and no longer functions as expected. What could be the...

ksd4692 by Associate II
  • 2114 Views
  • 6 replies
  • 2 kudos

STM32F401 Interpreting DMA data over serial

Hi all,I am pretty new to ST so bear with me.The controller is reading in voltage values into the ADC and sending to PC over serial withCDC_Transmit_FS((uint8_t*), buffer, buffer_length)I'm getting the data stream, but the values as read in python fo...

STM32F401CCU6 Crashes in empty while loop.

HelloI am testing new MCU's. I have a ST-Link V2 and using a STM32F401CCU6.At the start I had a simple LED flasher application however after I could not run it I started stripping everything out.This is when I saw that I can actually not even run an ...

STM32Issue1.png STM32Issue2.png
table by Associate II
  • 1709 Views
  • 4 replies
  • 1 kudos