STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4Discovery and debugger bug report

Posted on April 05, 2016 at 17:03Hi, The newly delivered STM32F4Dicsovery has debugger Firmware V2.25M14 on it. The same is on ST-Link utility V2 3.38. Both have following problem: When the board is powered up without USB on debug connection then th...

Osto by Senior
  • 1141 Views
  • 2 replies
  • 0 kudos

From mbed to offline IDE

Posted on April 05, 2016 at 06:17Hello.I would like to ask a question that might sound very basic almost silly to you, so my apologies.I am now programming a STM32F091 Nucleo board using mbed. (since it says ''mbed enabled'' and mbed is easy to lear...

d_aliaga by Associate II
  • 2195 Views
  • 3 replies
  • 0 kudos

Virtual COM Stm32fxx and complete transfer

Posted on March 23, 2016 at 10:41Hi, i'm using a virtual com (without uart), someone know the way to know when the usb has complete the transfer ?I can't make (sure) immediatly two time ''CDC_Transmit_FS''CDC_Transmit_FS( Buf, 100 );// here i need t...

Marco1 by Associate II
  • 720 Views
  • 1 replies
  • 0 kudos

stm32F071 + STOP MODE + wakeup + HSI48 = hard fault

Posted on April 05, 2016 at 10:31For a wearable product we're working on a device that wakes up 160 times a second (for now, will later be reduced to ~10 times per second), does it's thing, communicates with a host and remains in STOP mode for the r...

henk23 by Associate II
  • 2075 Views
  • 3 replies
  • 0 kudos

problems about STM32F446 TIM2 as External counter

Posted on April 05, 2016 at 15:49I'm using STM32F446RE NUCLEO and I need to count the external pulse.I don't know how to configurate it to enable the counter.the value of counter is 0 whatever the input fruquency.the following code is my configurati...

Place stemwin fonts in external flash

Posted on April 04, 2016 at 19:49Hello, I use stemwin with stm32f7 controller. I would like to put fonts and bitmap in external nor flash memory. I have declared my section in linker file. But I don’t know how to generate hex or bin file to put in n...

aurelien2 by Associate II
  • 1432 Views
  • 2 replies
  • 0 kudos

TIM CR2.CCDS functional?

Posted on April 01, 2016 at 20:54STM32 timers CR2 contains CCDS which seems to have no effect.  Reference manuals say that it selects DMA on update rather than compare.   DIER register contains DMA enables for all compares as well as update, so desc...

CubeMx creates some bugs

Posted on January 21, 2016 at 14:43CubeMx 4.12.0 Mcu: STM32L476RETx Fimware Package: L4V1.2.0 -Cube is generating code for port H, but there's no port H on the L476RET  /*Configure GPIO pins : PH0 PH1 */    GPIO_InitStruct.Pin = GPIO_PIN_0 | GPIO_PI...