cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO 5V in AF

fiulala
Associate II
Posted on November 19, 2015 at 19:03

Hi,

I wanted to know how could I have 5V in a pin associated with a timer. I do this configuration:

/*GPIOA Configuration: TIM9 CH1 (PA2)*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);

If I try this pulling up with a resistor to 5V, I only get 3,3-3,5V in PA2. If I do the same but in Output Mode i get the 5V. So, how could I get 5V if the pin is in AF?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Mikk Leini
Senior III
Posted on November 19, 2015 at 20:47

Hi,

Which microcontroller are you using?

Posted on November 19, 2015 at 21:30

For a static signal, I wouldn't expect GPIO/AF to make a difference, the control signals are upstream from the drive transistors.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
fiulala
Associate II
Posted on November 20, 2015 at 11:11

Hi,

Which microcontroller are you using? 0690X0000060MnQQAU.gif Sorry, I thought I had said that. I'm using stm32f4-disco.

For a static signal

... Well I don't want a static signal I'm associating pin PA2 to TIM9 to make a square signal. I do like this:

void TIM9_Configuration(void)

{

TIM_OCInitTypeDef TIM_OCInitStructure;

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

uint16_t Period;

Period = 100000 / 10; // 10 Hz for 100kHz prescalled

/* Time base configuration */

TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 100000) - 1;

TIM_TimeBaseStructure.TIM_Period = Period - 1;

TIM_TimeBaseStructure.TIM_ClockDivision = 0;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseInit(TIM9, &TIM_TimeBaseStructure);

/* Enable TIM9 Preload register on ARR */

TIM_ARRPreloadConfig(TIM9, ENABLE);

/* TIM PWM1 Mode configuration */

TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

TIM_OCInitStructure.TIM_Pulse = Period / 2; // 50%

TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;

/* Output Compare PWM1 Mode configuration: Channel1 PA.02 */

TIM_OC1Init(TIM9, &TIM_OCInitStructure);

TIM_OC1PreloadConfig(TIM9, TIM_OCPreload_Enable);

/* TIM9 Main Output Enable */

TIM_CtrlPWMOutputs(TIM9, ENABLE);

/* TIM9 enable counter */

TIM_Cmd(TIM9, ENABLE);

}