STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB HOST (type A) advice

Posted on April 06, 2016 at 12:43Hello everybody!I want a little advice on the best way to code (on a STM32F4) an USB HOST ''ONLY'' with a standard type A connector.The picture of the STM32 > USB CONNECTOR cabling is attached: https://my.st.com//pub...

STM32F103 CAN ERRI bit always set

Posted on February 28, 2016 at 17:43Hello,I have a problem with CAN bus on STM32F103TB.I have CAN_ESR register = 0 but still I get bit ERRI in CAN_MSR = 1.If i try clearing it either via code or via debugger it will be set again by hardware.I've sea...

SPLabs by Associate II
  • 2708 Views
  • 5 replies
  • 0 kudos

DMA

Posted on April 08, 2016 at 15:37Hi i wonder  if there is a way to transfer from pheripheral to pheripheral using dma on f429.could anyone tell me ?

arunease by Associate II
  • 1346 Views
  • 3 replies
  • 0 kudos

sizeof() function

Posted on April 08, 2016 at 21:21Hello.I would like to get a size of a struct in bytes. Members of a struct are different - concretely I have 6 WORDS and 1 array of 6 BYTES. Then, the size of a struct would be 30 BYTES. If I use function sizeof(stru...

matic by Associate III
  • 4319 Views
  • 7 replies
  • 0 kudos

Wrong clock frequency after IWDG reset [STM32F405]

Posted on April 09, 2016 at 12:42Hi all,I'm experiencing a strange problem on STM32F405When a IWDG reset happens, the uC restarts with a wrong clock frequency, I think it's running from HSI instead of HSE.  Same problem happens even if I call NVIC_S...

luigi23 by Associate
  • 990 Views
  • 1 replies
  • 0 kudos

Using SWD pin as as conventional IO?

Posted on April 08, 2016 at 23:55Can I, used SWD pin, for example on STM32F0, as SWD when debugging and flashing MCU and as little used IO , during normaloperation? If yes, how?

astrid by Associate II
  • 1432 Views
  • 2 replies
  • 0 kudos

Startup: why is .data alignment = 8

Posted on April 08, 2016 at 15:11Hello,while writing a bootloader, I had the need for a few bytes (4) that retain the content during a software reset. I�ve read that is true for the first bytes of the SRAM. So I�ve added a new section at the beginni...

torsten2 by Associate II
  • 3409 Views
  • 3 replies
  • 0 kudos

Manual DMA event triggering

Posted on April 08, 2016 at 09:51On the STM32F303 I have a timer with an OC that triggers DMA events to write byte values onto GPIO. The DMA is set up with a cyclical byte buffer that is populated by the core via interrupt. For technical reasons I n...

luke2 by Associate II
  • 1253 Views
  • 1 replies
  • 0 kudos